Part Number: CSD18535KCS Other Parts Discussed in Thread: CSD18536KCS , Hi Team, May we request for the lib file for CSD18535KCS? The lib file given on the PSpice model (slpm151a) present on its product page seems to be incorrect, as it is the lib file f…
Part Number: CSD18535KCS Other Parts Discussed in Thread: CSD , Hi team,
I wonder if CSD18535KCS is directly replaceable with FDMS3662. I checked those have the same pinout and similar package size, but it seems TO-220 of CSD is little different to TO-220AB…
Part Number: CSD18535KCS I'm using an optocoupler for using the CSD18535KCS as a switch. The input pulse to the optocoupler is 3.3V at 50KHz. The output from the optocoupler is a square wave as desired, but after connecting the terminals of the output…
Part Number: CSD18535KCS The package limited abs max Id current is stated to be 200A in the datasheet for this device. This seems large considering the size of the leads for the TO-220 package. Is the 200A rating only good for a fraction of a second?…
Part Number: CSD18535KCS Other Parts Discussed in Thread: TPS2828 , UCC27531 , LM5112 , CSD
i am not able to find an appropriate driver which can go from 3.3 to 10 V which is required for getting the low rds on of 1.7mohm. I am designing a boost converter…
Part Number: CSD18535KCS Other Parts Discussed in Thread: TINA-TI , Tool/software: TINA-TI or Spice Models Please provide tina simulation file for the abone part no. I am not able to run the given p-spice model. My LT spice software is latest one, but still…
Other Parts Discussed in Thread: CSD18535KCS Hi,
I used the CSD18535KCS.OLB and CSD18535KCS.LIB models by adding them to the implementation line in the "MbreakN" Mosfet part. I'm using two of the CSD18535KCS Power Mosfets to create a push-pull…
Other Parts Discussed in Thread: CSD18535KCS I'm trying to build a DC light controller and I'm having all kinds of problems. My setup is a 12 volt car battery and a headlight, I have the CSD18535KCS MOSFET on the low side and an Arduino send a PWM…
Other Parts Discussed in Thread: CSD18535KCS I'm building a simple switch for a 130A DC motor (locked rotor amps) and have purchased some NexFET power transistors (CSD18535KCS). I chose these for the low Rds value and high current. The Datasheet claims…
Part Number: BQ76952 Other Parts Discussed in Thread: CSD18535KCS Please give example of logic POWER MOSFET can be used on low side. Need for reference only. These will be driven directly by logic output 5V of DDSG & DCHG. I checked application report…