Part Number: CSD18537NQ5A Other Parts Discussed in Thread: TPS23753 Hi TI,
Can you determine the gain corner frequency of a TI FET(CSD18537NQ5A)?
I have the following problems.
PD 'TPS23753' review. (The circuit diagram refers to the TI 'PMP5220' reference…
Other Parts Discussed in Thread: CSD18537NQ5A Hi folks,
I got ESD test result for CSD18537NQ5A.
It was CDM=2kV, and HBM is 500V.
I suspect that the CSD18537NQ5A HBM is quite low, since other product's in TI shows around 1K~2kV.
Is the CSD18537NQ5A HBM…
Part Number: UCC27282 Other Parts Discussed in Thread: CSD18537NQ5A
Hi Gate Driver Team,
Can I ask some questions while running the UCC27282 PSPICE simulation (Transient model from the ti.com product folder)?
(1) When I run the simulation, I can see…
Part Number: TPS2493 Other Parts Discussed in Thread: CSD18537NQ5A , TPS2493 using design calculator managed to get the design summary [attached below]and values. But i need to understand the diagram if i need to add two or three MosFET [CSD18537NQ5A] in…
Part Number: LM3150 Other Parts Discussed in Thread: CSD18537NQ5A , CSD18504Q5A Hi,
I did a webench Design for a LM3150 21-30Volt input and 19V output.
After assembly and turning on the current limit of the Power supply who feed the circuit was maxed out…
Part Number: TPS2490 Other Parts Discussed in Thread: CSD18537NQ5A Hi,
We use TPS2490 in a load switch configuration for switching a voltage of 40-50V with a drain current requirement is max 1A. The output load cap is 3000uF. The MOSFET used is CSD18537NQ5A…
Hi Jackie,
I changed the part from CSD18504Q5A to CSD18537NQ5A and the problem went away. Now I can start looking into running the simulation.
You guys should probably look into that SPICE model.
Cheers,
Part Number: LM3150 Other Parts Discussed in Thread: CSD18537NQ5A , TINA-TI Hello,
I've created a shematic with the webench.
Vin=18 - 24 V
Vout=13,5V
Iout=12A
After that i tried to use the TINA TI transient model of the LM3150 (Rev. A) to simulate…
Part Number: LM5069 Other Parts Discussed in Thread: CSD19536KTT , CSD18537NQ5A Hello team,
Do you have a recommendation of TI FET used with LM5069?
Thanks in advance. S.Sawamoto
Part Number: TPS40170 Other Parts Discussed in Thread: CSD18504Q5A , CSD18537NQ5A , Tool/software: WEBENCH® Design Tools Good Morning,
We designed a system that utilizes the TPS40170. We used WEBENCH to design the system to set the voltage at approximately…