Other Parts Discussed in Thread: CSD18563Q5A Hi All,
I am not sure if this is the right place I should ask this question, if not, sorry for inconvience!
Our company have purchased total 80pcs CSD18563Q5A(first lot 60pcs and second 20pcs). We used more…
Part Number: LM3150 Other Parts Discussed in Thread: CSD18563Q5A , LM25145 Hi,
I am uisng LM3150 , so far it is good. But I am curious one thing for chip temperature.
Test setting is: 24V input, wihout loading, with the different output voltage.
The question…
Hi Yifan,
The Miller plateau voltage of the FETs should be in the range of 3V to 5V, so that 7.5V gate drive amplitude (= Vcc) provides adequate overdrive at turn on. What FETs are currently used? As an example at 60V, take a look at the CSD18563Q5A…
Other Parts Discussed in Thread: LM5118 , TINA-TI , CSD18563Q5A I am working on a re-design for an LM5118 Buck/Boost Converter. Webench recommends this FET as the HS FET. I would like to simulate in TINA-TI, which I simulated our old LM5118 Design. I'm trying…
Part Number: LM5145 Other Parts Discussed in Thread: CSD18563Q5A , CSD19534Q5A
HI All
We use LM5145 under the following conditions VIN=15V~36V VOUT=12V IOUT=5A FSW=300KHZ Ambient temperature up to 70 degrees MOSFET we choose CSD18563Q5A high-side and low-side…
Part Number: UCC24612 Other Parts Discussed in Thread: CSD18563Q5A , , TPS23756 Hello,
* I am using UCC24612-2 in flyback as Low-Side SR in 25W loading system, Vload = 5V. * I found that when the flyback system with Low-Side SR working at CCM (power loading…
HiZhang,
This is a 100V FET with high Rdson and hih Qrr. If Vin-max is 48V, thenyou can use a 60V FET. This will give lower power loss. Take a look at TI's NexFET portfolio of 60V FETs. In partiicular, you can use the NexFET calculator tool here: …
Part Number: LM5145 Other Parts Discussed in Thread: CSD18563Q5A , LM61480 Design Requirements:
Input Voltage Range: 9V - 36V
Output Voltage: 5V
Output Current: 8A
Max Allowable Voltage Ripple (peak to peak) : 100mV
Find the attachment below that contain…
Part Number: LM5143-Q1 Other Parts Discussed in Thread: LM5143 , , CSD18563Q5A LM5143-Q1.pdf
Can someone check if my schematic is correct? I have 48V input, and wanted either 24 or 36 Volt output. (selectable via Q6) But for some reason, the output is always…