Part Number: CSD19502Q5B Hi!
I wonder how can I calculate maximum power throw MOSFET and if needed the case junction, where to apply and how to calculate it.
Let's take CSD19502Q5B
It is written 3.4 mOhm and maximum continous current 100A (package…
Part Number: CSD19502Q5B Hi Team,
CSD19502Q5B VGS=10V, ID=50A Drain-source on-state resistance can under 3mΩ?
Infineon-BSC030N08NS5-DataSheet-v02_04-EN.pdf
Part Number: CSD19502Q5B Hi Team,
In one of our designs, we use a MOSFET CD19502Q5B. We couldn't find any information about the maximum current of the body diode in the datasheet. It would be extremely helpful if you could share the necessary information…
Part Number: UCC28C40 Other Parts Discussed in Thread: CSD19502Q5B , Dear,
we use UCC28C40 and CSD19502Q5B, power up moments, MOS peak current 8A, and then IC and MOS was demage.
schematic as below chart:
YIAPFJ1907T---- 0531.pdf
If any suggestion…
Part Number: CSD19502Q5B Hi Sir/Madam,
My customer is looking for SON5X6 package TI MOSFET. The lowest RDS(on) for TI SON5X6 MOSFET is 3.4mOhm(typ), 4.1mOhm(max).
Is there any other SON5X6 MOSFET with lower RDS(on) in roadmap which I can propose…
Other Parts Discussed in Thread: CSD19502Q5B Hi Can you please provide the following information for the CSD19502Q5B Part ?
1. Junction Temperature Max (Tj Max)
2. Typical Power dissipation (Pd typ)
3. Maximum Power dissipation (Pd max)
4. Thermal…
Part Number: LM25145 Other Parts Discussed in Thread: CSD19502Q5B , LM65640 Hey,
I using an LM25145 design of 28v to 3.3v at 4A with a 2.2uH inductor.
HS Mosfet-CSD18534Q5A ; LS Mosfet- CSD19502Q5B.
I found that the circuit is creating high Radiated…
Part Number: LM5101A Other Parts Discussed in Thread: CSD19502Q5B , Tool/software: I have not been able to get this circuit to work properly and convincingly with many MOSFET models.
VDD=10V VLI and VHI are complementary square wave inputs of 10 MHz…
Part Number: LM5176 Other Parts Discussed in Thread: PMP21278 , , CSD19502Q5B , LM51770
Hello,
We are facing a critical issue with LM5176 in a design based almost 1:1 on TI PMP21278 Reference design.
The only change compared to the reference design…