Part Number: CSD19533Q5A Other Parts Discussed in Thread: LM5069 ALL HI.
The figure below shows the data of thermal resistance provided in the CSD19533Q5A datasheet and the conditions for its implementation.If I use the same sheet FR4, copper foil thickness…
Part Number: CSD19533Q5A Hello,
can you provide something like "gate-drain oxide capacitance" and "drain voltage at which oxide capacitance becomes active" for CSD19533Q5A?
Regards,
Adam
Part Number: CSD19533Q5A Hello,
can I ask for unencrypted SPICE model of CSD19533Q5A but Level 3 ?
There is Level 7 on the website but it's not compatible with my software tool
Regards,
Adam
Part Number: CSD19533Q5A Other Parts Discussed in Thread: CSD19538Q2 , CSD Hello,
We are looking to understand the similarities between the CSD19532Q5BT and CSD19538Q2 MOSFETs in comparison to CSD19533Q5AT. We have previously done radiation testing…
Part Number: CSD19533Q5A Tool/software: The CSD19533Q5A has a 4-pin drain as shown in the image on the left below. However, what problems can occur if the PCB pad is designed with only 2 pins as shown in the Gerber image on the right below?
Part Number: CSD19533Q5A Other Parts Discussed in Thread: LM74700-Q1 , , CSD18510Q5B , CSD18540Q5B , CSD19536KTT , CSD88584Q5DC Hi, Support Team.
I plan to use two LM74700-Q1 to achieve ORING function, the input power is DC 18V~32V, the regular voltage…
Part Number: CSD19533Q5A Hi Experts,
My customer is asking about the peak I_DS. There is a chance that a I_DS flows over 231A which violates abl max of this FET when a failure occurs. Customer wants to know if this pulse peak current is acceptable.…
Part Number: CSD19533Q5A My client is working on a board design using CSD19533Q5A & we need unencrypted Spice model to perform simulation on Simetrix platform. We do have global NDA covered with end customer for this case. Thanks & look forward to hear…
Part Number: CSD19533Q5A Other Parts Discussed in Thread: CSD17578Q5A , Hi, Greetings. Our customer noticed that the recommended PCB pattern measurement doesn't add up. They tried to compute the value of F3 to ensure the measurement. When using the min…