Part Number: PSPICE-FOR-TI Other Parts Discussed in Thread: CSD19535KTT , CSD19535KCS Hello,
I run into "Name on .ENDS does not match .SUBCKT" error with TI part CSD19535KTT and I checked the related thread to solve this problem.
Could you help…
Part Number: CSD19535KTT Hello,
I'm using CSD19535KTT for BLDC Motor control application,
Voltage 48V and Peak Current 42A
I have gone through the TI training videos and blog post regarding MOSFET selection,
As mention in datasheet Rds on 3.2mOhm…
Part Number: CSD19535KTT Hi Team,
customer using CSD19535KTT and found some pcs that due to leakage current too high and there is a remaining voltage present even with the FET is turned off.
resulting the output voltage will still turn on the remaining…
Part Number: CSD19535KTT hi Team,
it's reported by our customer on one of the CSD19535KTT IC
it's observed that the VDS leakage current will increase over time, can we have your comment on this?
VGS:200kohm
VDS: 28.8V
monitor VDS current:
…
Part Number: CSD19535KTT How can I achieve good heat rejection of Power MOSFET CSD19535KTT with D2PAK package?
While comparing to the base area of MOSFET, I am increasing the copper area on the PCB like 10%, 20%, 30% and so on.
while doing like that…
Part Number: CSD19535KTT Hi Team,
the datasheet specifies the following thermal resistance.
Can you please specify in more detail in respect to which part of the case (i.e. top or bottom) the parameter is given ?
Do you have thermal heat maps…