Part Number: CSD19538Q2 Other Parts Discussed in Thread: TINA-TI Hi Experts,
I noted the drain-to-source leakage current (in off state) is always specified at <1uA @ 80Vds, 0Vgs. I am guessing this 1uA spec is just a test criterial, instead of real leakage…
Part Number: CSD19538Q2 Hello,
I am using the CSD19538Q2 as a low side switch for controlling a solenoid. I am driving it using an MCP1416 gate driver which can source/sink at 1.5A peak current with a drive voltage of 12.9V at a PWM frequency of 24kHz…
Part Number: CSD19538Q2 Other Parts Discussed in Thread: LM5146 , In my LM5146 design, my high-side FET is the CSD19538Q2 which has around 0.6W of loss in the 2x2mm package. Is this too much loss for that small package to handle? Also, the thermal resistance…
Part Number: CSD19538Q2 Dear Team
The customer would like to know the difference between CSD19538Q2 and CSD19538Q2 T
Could you help to recommend?
Many thanks
Denny
Part Number: CSD19538Q2 Other Parts Discussed in Thread: TPS43060 Hi Team,
The Webench model for the CSD19538Q2 shows a Qrr of 0nC, resulting in incorrect efficiency numbers for some controller designs. Can the model be updated?:
Thanks,
Antonio
Part Number: CSD19538Q2 Other Parts Discussed in Thread: CSD16301Q2 , CSD17571Q2 , Hi,
My customer need below auto grade MOS. please kindly recommend accordingly. thanks.
CSD16301Q2_25V_5A_TI
CSD17571Q2_30V_22A_TI
CSD19538Q2_100V_14.4A_TI
…
Part Number: CSD19533Q5A Other Parts Discussed in Thread: CSD19538Q2 , CSD Hello,
We are looking to understand the similarities between the CSD19532Q5BT and CSD19538Q2 MOSFETs in comparison to CSD19533Q5AT. We have previously done radiation testing on the …
Part Number: CSD19538Q2 Hi Team,
Customer is asking about the parameters of the diode integrated in CSD19538Q2, such as the forward current range, the forward voltage.
Looking forward to your reply. Thank you!
Marc