Part Number: BQ2970 Other Parts Discussed in Thread: CSD83325L , BQ2980 I’m curious about the FET choice because our over-current thresholds are going to be very low (250-350mA). I originally picked a small FET (CSD83325L) to start and with 20mΩ Rds,on…
Part Number: BQ27742-G1 Other Parts Discussed in Thread: CSD87501L , CSD83325L Hi team,
Can you have a look at the following customer issue please? Is there a MOSFET that you recommend to use with BQ27742-G1 instead of uPA2375T1P or CSD87501L?
We…
Hello,
I am not sure about it. I think it is 1S.
We have 3 cells in parallel. Each having capacity of 3000mAh and a termial voltage at full charge of 4.2V.
We have BQ29700DSET and CSD83325L for battery protection.
Part Number: TIDA-00712 Other Parts Discussed in Thread: CSD83325L Hi,
We are evaluating battery protection designs for a new wearable device and are currently considering using the BQ29700 coupled with the CSD83325L (similar to the TIDA-00712 reference…
Other Parts Discussed in Thread: CSD13380F3 , CSD83325L Hi!
I am designing BMS design for research purpose. for that i cannot explain the whole idea but i need to control the charging and discharging of single lithium ion cell.
For this purpose i…
Part Number: BQ2970 Other Parts Discussed in Thread: TIDA-00712 , , BQ25120 , CSD83325L I have made a circuit design that very closely mimics the TIDA-00712 reference design. Long story short, my battery is always connected to the circuit and I am seeing…
Part Number: BQ27742-G1 Other Parts Discussed in Thread: CSD83325L What's the limiting factor for current for this solution? It seems it would be the FETs chosen and the sense resistor's power handling capability. However I noticed the eval board is limited…
Part Number: BQ2970 Other Parts Discussed in Thread: CSD83325L , CSD85302L Hi,
We are working on an application for a wearable device that utilizes an extremely small capacity lithium polymer cell (30mAh) and completes the battery protection circuitry…
Hi Onyx,
Thanks for the prompt reply. The IC you mentioned looks fine. Similar to what my requirements are. I went through the datasheet where the FET mentioned (CSD83325L) has max ID value of 8A. Though my application will be around the mark of 5A …
Other Parts Discussed in Thread: CSD13383F4 , CSD83325L , CSD13302W , CSD13306W , CSD15380F3 Hello all,
I have a unit with following input power supplies: (1) +7V with 0.4A, (2) +5V with 0.2A and (3) -5V with 0.06A.
I have to switch-off the unit with…