Part Number: CSD87330Q3D We are using one part ( part no CSD87330Q3D ) in our design and we need the thermal data for this part for thermal simulation
Kindly provide the below thermal details for this parts as these values are missing in its datasheet
…
Part Number: CSD87330Q3D Other Parts Discussed in Thread: CSD87350Q5D Dear TI,
We use TI's CSD87330Q3D, and we need to fill out their own form for reliability team.
They requested us to share the ESD spec, but we can't find on the datasheet and TI webpage…
Part Number: TPS51285B Other Parts Discussed in Thread: CSD87335Q3D , , CSD87330Q3D , CSD87351Q5D Hi,
We have 5V/24A application, does power block CSD87335Q3D is suitable for TPS51285B 5V output?
We have used CSD87330Q3D(20A cons.) is proviuos project, but…
Part Number: CSD87335Q3D Other Parts Discussed in Thread: TPS51285A , CSD87330Q3D , i have designed a 3.3V/5V converter using TPS51285A.
i have selected CSD87330Q3D for the design. input voltage is 8.4V -12.6V. output current is 15A. OCP value set as 18A. Inductor…
Part Number: CSD87330Q3D Hello,
I'm designing a project that include CSD87330Q3D along with TPS65911A.
In the reference design, the input voltage for the CSD87330Q3D is 12V. in the typical application wrote Max. 12V Input. I'll like to supply 5V to…
Part Number: CSD87330Q3D Other Parts Discussed in Thread: CSD87335Q3D , CSD87333Q3D , CSD87334Q3D , CSD86330Q3D , CSD86336Q3D , CSD87331Q3D , CSD17302Q5A Hi Team,
My customer is using CSD87330Q3D but its ESD rating is only 200V. Do we have P2P or similar solutions…
Part Number: TPS59641 Other Parts Discussed in Thread: CSD87330Q3D , CSD87334Q3D , Hi sirs,
We test the VCC(Vcore) dynamic VID measurement change Mosfet from csd87330q3d to csd87334q3d
test condition:
Vmax
1.150 V
Vmin
.7 V
Static Icc
5 A
SVID…
Part Number: TPS51285A Other Parts Discussed in Thread: CSD87330Q3D Hi Team,
Could you please help suggest the selection of MOSFET of TPS51285A/B? Do we have any specific requirement such as Rdson etc?
Best Regards,
Jaden Yue
Part Number: CSD87330Q3D Other Parts Discussed in Thread: CSD17309Q3 Hi, I would like to ask about CSD87330Q3D SOA data. Customer wants data like the following. However, there is no description of that data in the data sheet. Does CSD87330Q3D have such data…