Other Parts Discussed in Thread: DRV8320 , CSD86336Q3D , CSD87330Q3D , BOOSTXL-DRV8320S , CSD88599Q5DC Hello,
My current design for 3 phase BLDC motor driver is DRV8320 with 2 FDMC8010DC (On Semi) on each phase. Motor is 16V, 15A maximum.
Filtering NextFet…
Part Number: TPS650864 Other Parts Discussed in Thread: CSD87330Q3D Hi,
We are trying to use TPS650864 to supply a Xilinx ZYNQ Ultrascale ZCU7EG.
However, we have tried a lot of L/C combinations, but have never been able to start correctly the power supply…
Part Number: TPS65911 Other Parts Discussed in Thread: CSD87330Q3D , EVMK2GX , 66AK2G12 , Hello, customer is in a design with the 66AK2G12. They want to use the TPS65911A to power it. They have a question regarding powering the external FETs for VDDCtrl SMPS…
Part Number: LM5175 Other Parts Discussed in Thread: CSD87330Q3D Hi Team,
We would like to use LM5175 for USB PD at the following conditions.
INPUT: 12V
OUTOUT: 5V/3A, 9V/3A, 12V/3A, 15V/3A, 20V/3A, 20V/5A
Then, we need Small and Low cost solutions…
Hello,
Thank you! We had chosen the mosfet based on our size requirements.... as it is a small board..
We need something 3.3mm x 3.3mm or smaller.
Is CSD87330Q3D acceptable? (9.3-11mohm RDSon)
Thanks!
Hi Akshay,
Thanks for the inquiry. The CSD58873Q3D is a custom part number. The commercial part number is CSD87330Q3D. This device passes 200V HBM & 1000V CDM. TI does not do MM ESD testing of our FETs and power blocks.
Part Number: CSD86350Q5D Other Parts Discussed in Thread: CSD87330Q3D , , CSD16407Q5 , CSD17575Q3 Hi Team,
Our customer would like to know Transient thermal resistance vs Pulse Width Graph of CSD86350Q5D and CSD87330Q3D.
Could you please let us know if…
Hello,
This is Akshay from Flex India.
We are currently working with one of our manufacturing plant to collect ESD(Electrostatic discharge) information.
The list for the required part no is attached.
Please help to provide the details ESD..xlsx .
Thanks…
Part Number: TPS53219A Other Parts Discussed in Thread: CSD87330Q3D , , TPS51219 Hi,
I have new request as follows:
20V nominal input, max acceptable up to 24V
Max output current= 15.5A
Output voltage= 0.9V
Transient 0.8A =>7.3A in 2us (6.5A inrush in…
Part Number: LM5175 Other Parts Discussed in Thread: CSD87330Q3D ,
Hi Sir,
May I know LM5175 controller suitable use CSD87330Q3D Power Block MOSFET? since currently we have board size issue.
Please help comment this schematic, thanks.
LM5175 with CSD87330Q3D…