Part Number: CSD87355Q5D Hi Team,
Please share the qualification summary report for the part CSD87355Q5D
it is not available in Ti website:
www.ti.com/.../home
Awaiting for your quick response.
Please do the needful at the earliest.
Kindly…
Part Number: CSD87355Q5D Hi Team,
What is the ESD Rating & Model?(for ex: HBM = 8kV) for the part number CSD87355Q5D
What is the Technology & Process node?(for ex: CMOS, 80nanometer (nm))?
Awaiting for your quick response.
Please do the needful…
Part Number: CSD87355Q5D Hi Team,
good day.
this is regarding the part number: CSD87355Q5D, in which there is difference between the datasheet vendor recommended land pattern and the package code DQY0008A vendor recommended land pattern, kindly check…
Part Number: CSD87355Q5D Tool/software: Hello experts
Hope this finds you well.
Do we have higher voltage and P2P device for this please?
60V is needed.
We use this as FET for TPS51215ARUKR.
Thank you
Regards,
Zhou
Part Number: CSD87355Q5D Hi Support Team.
I have a question about 「9.1 Q5D Package Dimensions」 in CSD87355Q5D's data sheet.
Does "Exposed Tie Bar May Vary" exist only in Front View?
Does it also exist on the other side?
Thanks,
Part Number: CSD87355Q5D Other Parts Discussed in Thread: TPS51219 , TIGER Hi,
If my application will switch different Vin between 12V in 5V, is there any risk and side effect that have to consider in design?
In S0 power state, VIN will be 12V.…
Part Number: CSD87355Q5DCSD87355Q5D VGS question :
CTMR like to ues CSD87355Q5D for Half bridge power stage and H/L side driver voltage is 12V, But CSD87355Q5D recommond driver reange is 4.5~8V, please helo offer suggest to slove this Issue.
Part Number: CSD87355Q5D Other Parts Discussed in Thread: CSD18510Q5B Hi Team,
In the Feature, there is a description saying that, "High-Frequency Operation (Up to 1.5 MHz)". May I know where frequency limit comes from? And, what will happen if the…
Brett,
my original question actually was without a heat sink (or maybe if Webench already is using a heat sink since they use a much lower value).
When I use these 50 °C/W the junction temperature reaches its limit rather fast, therefore, I asked…