Part Number: CSD18540Q5B Other Parts Discussed in Thread: CSD88584Q5DC , TIDA-010042 Tool/software: hi
CSD18540Q5B has a thermal pad on the bottom, but does not have any suggestion about thermal vias. Is this part not recommended to have thermal vias…
Part Number: DRV8323 Other Parts Discussed in Thread: TIDA-00774 , CSD88584Q5DC , TIDA-01516 Tool/software: Hello, I'm using the DRV8323S coupled with the CSD88584Q5DC mosfets much like the TIDA-01516 and TIDA-00774 reference designs, yet when I attempt…
Part Number: CSD88599Q5DC Other Parts Discussed in Thread: TIDA-01485 , CSD88584Q5DC , TIDA-00774 Tool/software: Dear TI,
I am puzzled by the datasheet information that why is the potential of the top "EXPOSED HEAT SLUG".
Do it connected to the…
Part Number: DRV8412 Other Parts Discussed in Thread: DRV8320 , CSD88584Q5DC , Hi,
We are using the DRV8432 driver for years to control two L-C tank resonators, one for each Full Bridge. As known DRV8432 is obsolete and we are looking for an alternative…
Part Number: DRV8306EVM Other Parts Discussed in Thread: CSD88584Q5DC , DRV8306 ,
Hi,
My company makes a range of products which use BLDC motors. The control board for this range uses a DRV8306 coupled with 3 x CSD88584Q5DC to drive each motor,…
Part Number: DRV8306 Other Parts Discussed in Thread: CSD18514Q5A , CSD88584Q5DC Hi,
I would like to understand how to calculate R_ISEN?
In the EVM it is set to 0.007Ohm but I do not know the pulse by pulse current limit based on it.
From what I…
Part Number: BOOSTXL-DRV8323RH Other Parts Discussed in Thread: CSD88584Q5DC , CSD88599Q5DC Hello, BOOSTXL-DRV8323RH in the user manual, say that the MosFET packs used are the CSD88584Q5DC that have a maximum of 40V (top drain to bottom source). The Boost…
Part Number: DRV8306 Other Parts Discussed in Thread: CSD88584Q5DC I used the drv8306 in a portable device.
12V DC power supply for motor.
- 50W power output
- following is my circuit.
- 8000rpm ~ 30000rpm speed control
- 15K PWM
- mcu:STM32BOG1RCT6…