Part Number: CSD88599Q5DC Hi,
Typical Tr and Tf of CSD88599 is shown in the datasheet. What is the min and max value at the same conditions which are VDS=30V, VGS=10V, Rg=0ohm, and IDS=30A?
Best Regards, Taki
Part Number: CSD88599Q5DC Hi,
Could you explain the difinition of Tx in the datasheet and how to use in thermal design? The definition could not be found in the datasheet.
Best Regards, Taki
Part Number: CSD88599Q5DC Hi John Wallace1 ,
This is LEBA from NIDEC Corp.
I am under support by TAKIGASAKI ISAO.
May I ask you two question related to DMM0022A package of CSD88599Q5DC.
1) I got the CSD88599Q5DC_DMM_22.bxl file from TAKIGASAKI already and…
Part Number: CSD88599Q5DC Other Parts Discussed in Thread: CSD95379Q3M , DRV8305-Q1EVM , DRV8305 Hello
· We understand that your MOSFET Power Switch CSD19538 is rated to serve applications that require 100V-5Amp. Is that correct?
· We also…
The Qgd is 7nC, I don't really have a rise time target, but I wouldn't go too low on the slew rate, otherwise the fets could get really warm. I'm using TI's CSD88599Q5DC half bridge. What IDRIVE setting would you use for this? Thank you. …
Part Number: CSD88599Q5DC Other Parts Discussed in Thread: PMP21278 , Hi team,
My customer is thinking of implementing this reference design in their system, but the FETs are pretty pricey.
Can the above FET module replace the four FETs on the input stage…
Hi Patryk, CSD87334Q3D is a power block designed rather for DC/DC buck converters, I think a better option would be half-bridge like CSD88584Q5DC or CSD88599Q5DC. Regards, Grzegorz
Part Number: CSD88599Q5DC
I wanted to continue using thread https://e2e.ti.com/support/applications/motor_drivers/f/38/p/631056/2328299?tisearch=e2e-sitesearch&keymatch=CSD88599Q5DC#2328299
but it is locked.
So, is there another half bridge for replacing…
Part Number: CSD88599Q5DC Hi,
I used figures 1,4,5,6,19 and section 6.7.2 of the CSD88599Q5DC MOSFET datasheet to estimate power loss but this number is far larger then my calculation based on TI application report SLVA504.
Knowns: VIN = 24V, DC = 50%…