Other Parts Discussed in Thread: CSD95372BQ5M Hello,
(1) I am trying to use the CSD95372BQ5M as a boost regulator, is that possible?
(2) Why is the output of the CSD95372BQ5M limited to 5.5V? I'm not sure I even understand the metric, since V_sw alternates…
Hello,
Can you please provide more information about the IOUT and VREF pins? Namely, how can I use them to determine the amount of current flowing through the device? For example, what are their min/max values, what is the sensitivity of iOut (for example…
Part Number: CSD95377Q4M Other Parts Discussed in Thread: CSD95372BQ5M , You can clearly see the wires in the image of CSD95372BQ5M, but you can't see CSD95377Q4M at all.
Originally, the wire should be flying from the chip on the left side like CSD95372BQ5M…
Part Number: TPS40425 Other Parts Discussed in Thread: CSD95372BQ5M , TPS40428 Hi Team,
The customer report that the TPS40425 will enter the OTP when the device is only 60 degrees, we think that it should be they add the pull low resistor (PR6 and PR30…
Hi,
We do not suggest to operate with REFIN shorted to GND. but if you short the REFIN pin to GND, neither CSD95372BQ5M nor CSD95490Q5MC will break.
Best,
Qingquan
user4263612 said:
Please tell me about CSD95372BQ5M in the same series.
1. When the REFIN…
Part Number: TPS53647 Other Parts Discussed in Thread: CSD95372BQ5M , CSD Hello. I need help with running TPS53647. This is my first time using it.
When I make scheme and pcb, I referenced them from results WEBENCH Power Designer.
But it is not working…
Hi Reed Kacz,
Currently, the power stage is fixed to CSD95372BQ5M in Webench. this cannot be modified directly. I'll move this thread to the applications team, so that they can look into the possibility modifying power stages.
Regards,
Vishwanath …
Part Number: TPS53641 Other Parts Discussed in Thread: CSD95372BQ5M TPS53641 has VR_FAULT# asserted low. the fusion shows VIN_OV_FAULT_LIMIT (register 0x55) to be 15.000, with HEX value of 0x000F.
This is the only item that is different from a good working…
Part Number: TPS53667 Other Parts Discussed in Thread: TPS53647 , CSD95372BQ5M , CSD95490Q5MC , TPS40425 Hi Sir
the TPS53647 (4 phase) and TPS53667 (6 phase) are P2P solution. May we know what different between these 2 device?
The customer request around…