Part Number: CSD95373AQ5M Tool/software: Hi This is the Simulation Scheme with PSPICE for TI (Tj 125°)
The parameters set in accordance with the Datasheet (Output Current 23A)
According to the Datasheet Power Loss of 2.8 W is expected. But the PSPICE…
Part Number: CSD95373AQ5M Hello TI Team
The bootstrap capacitor is loaded every time, the Sync FET (lower switch) ist switched on, I think.
In the datasheet, there is a recommended "on time duty cycle" of 85% at fsw = 1 MHz. If there is a lower…
Part Number: CSD95373AQ5M Hi, Support Team
We saw the CSD95373AQ5M datasheet 9.1.1 recommended schematic overview
C16 and R2 show DNP, if i add C16 and R2 could help for EOS issue?
if any suggestion. Please advise me.
Thanks,
Best regards,
Lawrence
Part Number: CSD95373AQ5M Other Parts Discussed in Thread: CSD95373BQ5M , CSD95372AQ5M Hi team,
My customer has CSD95373AQ5M shortage issue and asks our help.
1. CSD95373BQ5M replace CSD95373AQ5M with REFIN & IOUT NC?
2. If B can't directly replace, any…
Part Number: CSD95373AQ5M Hi there,
I have a quick/basic question on DEM of CSD95373AQ5M.
Can you explain the difference between the operation of dead time and the operation of DEM? I'm confusing them. Simply put, both are just turning off HS FET and…
Part Number: CSD95373AQ5M Hi, Customer wants to install a 2.2kΩ resistor on VDD. In the background, the customer is trying to check the rated power of the resistor. Could you tell me the maximum value of VDD operating supply current?
Regards, Yusuk…
Part Number: CSD95373AQ5M Other Parts Discussed in Thread: DRV595 , Looking at the data sheet for this power stage I am left wondering how the power loss of the part varies at voltages approaching the power supply rail as this data is not shown (see the…
Part Number: CSD95373AQ5M Hi, Could you tell me the recommended VIA layout dimensions on the thermal pad?
There was no description of the via size in the data sheet. Customers want information similar to the following: Regards, Yusuke
Part Number: CSD97394Q4M Other Parts Discussed in Thread: CSD95373AQ5M Dear Specialists, Customers need FMEA information to adopt new parts. Please tell me the FMEA information of CSD95373AQ5M and CSD97394Q4M. It helps in design-in.
Best regards, Yusuke