Part Number: TPS53676 Other Parts Discussed in Thread: CSD95377Q4M , TPS544E27 Hi, In order to generate 0.3V, 25A output i was thinking of TPS53676 together with CSD95377Q4M. Is that a reasonable choice?
Part Number: CSD95377Q4M
Dear Sir,
About Absolute maximum ratings of Vsw to PGND(10ns).
Does it mean CSD95377Q4M can allow negative voltage over -0.3 under -7V in 10ns and positive over 20V under 23V in 10ns?
Since I measure the Vsw to PGND waveform…
Part Number: CSD95372BQ5M The undershoot of the waveform measured at the VSW pin meets the Absolute Maximum Ratings "VSW to PGND (10 ns) min -7V" of -7V, but not 10ns. Please provide offline support to check if there are any problems with the waveform…
Part Number: CSD95377Q4MCSD95377Q4M is a boost topology, The bootstrap capacitor provides the charge to turn on the control FET.If the capacitor can not be charged, CSD95377Q4M will it fail to start?
Part Number: CSD95377Q4M Other Parts Discussed in Thread: CSD95372BQ5M , You can clearly see the wires in the image of CSD95372BQ5M, but you can't see CSD95377Q4M at all.
Originally, the wire should be flying from the chip on the left side like CSD95372BQ5M…
Hi Minkyung,
I am not very sure about what exactly do you mean by "total capacitance".
The Vin capacitors are needed for: 1. limit voltage ripples on Vin; 2. provide energy buffer for power stages during transient; 3. some Vin caps are placed very…
Part Number: CSD95377Q4M Other Parts Discussed in Thread: UCD9224E , UCD9246E , UCD9248E , UCD9222 , UCD9244 , UCD74120 , UCD9246 , UCD74111 Is CSD95377 easily compatible with UCD924x digital controllers?
It looks like they would match up well, I believe…