Part Number: CSD95378BQ5M Hello
I have a 50A design using the CSD95378BQ5M. I have 6 boards that are working fine and 10 that are not.
The only difference is the date codes..... The current draw is very low at less than 2A
The ones that are working have…
Part Number: CSD95378BQ5M Other Parts Discussed in Thread: TPS40428 Hi
My customer has question.Please Cooperate me.
Voltage was generated in VDD when CSD95378B was operated under the following conditions.
VIN=12V
EN=0V
VDD=OPEN
When measuring the voltage…
Part Number: CSD95378BQ5M Other Parts Discussed in Thread: TPS40428 ,
I have a design that uses two CSD95378BQ5M connected through 220 nH inductors to generate a common VCCINT power supply. They are controlled by the TPS40428, but the VDD and ENABLE pins…
Dear Sir,
Please refer to attached excel file and please update me each TI spec and manufacturer part number with SMT Re-flow Thermal Profile. Thank you.
Best Regards,
Elyse Chou TI List 0531.xlsx
Other Parts Discussed in Thread: CSD16570Q5B Will be using the CSD95378
This is a output stage for a switching power stage. It has an H Bridge on the output side that can drive a lot of current.
It would drive a step up transformer that would drive the…
Part Number: TPS40428 Other Parts Discussed in Thread: CSD95378BQ5M if i am using a single 5V supply for a multi phase design can i trust the controller and power stage to power up and down together or do i need to delay the the controller to make sure…
Hello Nastasha,
I could see around 21A in fusion power design, system monitor.
Now we got different issue in another card - CSD95378BQ5M was damaged during power cycle test at 55C.
Please find the attached circuit - which was modified for better ripple…
Part Number: CSD95372BQ5M Other Parts Discussed in Thread: CSD95378BQ5M I have two questions:
(1) What's the difference between CSD95372BQ5M and CSD95378BQ5M? I cannot tell from the published datasheet.
(2) What's the gain (mV/A), offset, noise, and…
Part Number: TPS40428 Other Parts Discussed in Thread: TINA-TI , , CSD95378BQ5M Tool/software: TINA-TI or Spice Models FW a new high current DC- DC power convertor - TPS40428.msg
Hi TI Expert
we are looking for a new power DC- DC power convertor, for…