Part Number: CSD95410RRB Other Parts Discussed in Thread: CSD95372BQ5MC Tool/software: Dear Team,
Could you provided simplis model of CSD95410RRB and CSD95372BQ5MC?
I want to do simulation to check the dynamic performance.
Many Thanks,
WANG…
Part Number: CSD95410RRB Hello,
Is there a non-op temperature rating for these two parts? I did not see this mentioned in the datasheet.
CSD95410RRBT
TPS53688RSBT
Thanks,
Nate
Part Number: CSD95410RRB thermal engineer here. The datasheets for the both the csd95410 and 420 have a brief temperature range mention under the table Packaging Information. there the "op temp" is listed as -40 to +125 C.
there is no mention if this…
Part Number: CSD95410RRB Other Parts Discussed in Thread: TPS53681 Dear TI Team, I am planning to use CSD95410RRB with TPS53681 in my design. Could you please share the detailed datasheet for the CSD95410RRB part?
I checked online and able to find one…
Part Number: CSD95410RRB Tool/software: Hi
We want to do the thermal simulation of CSD95410RRB. Could TI share the method to calculate the thermal dissipation of CSD95410RRB?
Its Vout is 0.85V and Iout is 35A. Thanks.
KeHsu
Part Number: CSD95410RRB Other Parts Discussed in Thread: TIDA-010241 Tool/software: Hi,
I'm starting a new design using the CSD95410RRB device and I noticed the datasheet doesn't have any pinout information in it at all. How can I obtain the pinout…
Part Number: CSD95410RRB Other Parts Discussed in Thread: CSD95565 , TPS536C9T Hi,
I’m working on building a multiphase buck converter using the CSD95565 power stage. At the moment, I’m building it for open-loop mode (without a control IC), and I have…
Part Number: CSD95410RRB Other Parts Discussed in Thread: TPS536C7EVM-051 , CSD95410RWJ Hi,
I am using the TPS536C7EVM-051 for evaluation and I see it uses CSD95410RWJ NextFET powerstage. May i know the on resistance of the CSD95410RWJ for both top…
Part Number: CSD95410RRB
Tool/software:
Hi Abishek,
I have a follow up to the original question. What do you mean by "The RLSET value will be changed for the same inductance value."
Do I have to change the Rlset Value from e.g 105k for 150nH …
Part Number: TPS53681 Tool/software: Hi TI Team,
I am planning to use TPS53681 + 3x CSD95410 solution for my design to power the SoC core voltage.
Below are my design requirements:
Input voltage: 12V Output voltage: 0.75V Output current: 60A
I…