Part Number: CSD95495QVM Hello,
Can two CSD95495 power stages operate in parallel? Will the differences in gate driver delays cause problems? I could not find any gate delay specifications in the data sheet.
Thanks,
Chuck Sampson
Part Number: TPS53681 Other Parts Discussed in Thread: CSD95495QVM , Hi,
For some thermal concern of CSD95495QVM, we would like to do some experiment to just put max load 25A on one phase and check if need to add thermal solution for it.
Is there any way…
Part Number: CSD95495QVM Hi Team,
Is there any way to check " the temperature of CSD95495QVM use in Ta=45°C with power loss 2W&4W " and the junction-to-ambient thermal resistance of CSD95495QVM?
Part Number: CSD95495QVM Dear TI Team,
I am considering using CSD95495QVM as a half bridge in my design recently. The application is not buck converter, so actually I don't need the function of some pins like VOS, IOUT, LSET and TAO. I notice that the…
Other Parts Discussed in Thread: CSD95495QVM , CSD95492QVM The CPU solution is denverton, and the vid version is vr13,
The requirements are as follows: the maximum power consumption is 30W, and four power supply channels are required.
Pvcc 1.05v 30A svid_…
Hi Vikas,
CSD95495QVM or CSD95496QVM both meet your requirement. The optimal FSW is 600kHz for these parts, however, you definitely can select other frequency by different application as well.
Thanks
Chasel