Part Number: CSD97395Q4M Hello,
I have questions regarding the Gate-Treiber CSD97395Q4M, and I hope that you can answer these.
According to the datasheet, the recommended PWM should be 85%.
The measurements show a drop in performance only from 95%.
…
Thank you.
Indeed, DC-DC buck on each side of the TEC is what I want to do. The reason I'm investigating the CSD is that I can't find ready-to-use DC-DC with matching source / sink capability. The DC-DC I investigated can ALL source much more than…
Part Number: CSD97395Q4M Hi,
I have some issue using CSD97395Q4M. In the spec it says a tri-state (high impedance) on SKIP pin will put it in low power mode, and the tri-state voltage is 1.3-2V with 5V supply. However when I drive it with a 3.3V pin on…
Part Number: CSD97395Q4M I'm having issues with the output being disabled (100% DUC on PWM input, with no output). I think the chip might be going into UVLO mode or something else. My main culprit is the 5V line. It's a 1.5A supply, but on bootup, at…
Part Number: CSD97395Q4M Other Parts Discussed in Thread: BQ500215 Hi
I am using CSD97395Q4M like the typical application as power Stage for wireless charger with some parameter changes.
I want to know what is efficiency that this component is design…
Part Number: CSD97395Q4M Hi team,
Do we have the replacement for TLF11251LD?
https://www.infineon.com/dgdl/Infineon-TLF11251LD-DataSheet-v01_02-EN.pdf?fileId=5546d46276fb756a0177241a02695830
Part Number: CSD97395Q4M Other Parts Discussed in Thread: CSD97374Q4M Hi Team,
Could you pls inspire us what's the difference between CSD97374Q4M and CSD97395Q4M? I checked the d/s, which indicates it's nearly same. Thanks.
Best,
Stanley
Part Number: CSD97395Q4M Hi,
My customer is developing a product using CSD97395Q4M.
Please confirm your inquiry regarding the circuit below.
1. I want to change the capacitance value of the capacitor connected to the boot pin from 1uF to 100nF, is there…
Part Number: CSD97395Q4M Dear all,
I would like to ask a question.
Our customer asks if CSD97395Q4M falls under REACH.
If you check the web page of the product, you will see Pb free (RoHS Exempt).
I have heard that RoHS regulations do not apply even…