Hi Arakel,
Thanks for using the e2e forum, let's see if I can shed some light on some of the issues you are having.
The first thing I noticed with your design is that you are powering the DAC with +/-36V. This far exceeds the maximum supply ratings…
Viktor,
Sorry - evidently I misread the earlier message about a buffer and interpreted that as an interest in a DAC without an output buffer (amplifier).
DAC0800 is pretty unique in not having any latch mechanism for the input data. In most cases…
Hi Uttam,
As per Figure 01 ,I made circuit i got somehow analpg output w.r.t digital in.
What i did is i just removed my opamp block. Why my opamp block is not working??
In dac0800 datasheet
Fig.22 basic bipolar output operation
Fig.23 Symetrical…
Can you tell me more about this device. I am trying to output a digital signal (8-bit) to the DAC and get the corresponding analog signal. When I output "127", I get "0V" from the DAC, when I output "0", I get "5V" from the DAC. Is this do to the formatting…
Part Number: DAC0800 Hi,
We are using DAC0800LCM in our design and need to perform SI analysis.
Can you please let me know if any IBIS model is available for DAC0800LCM?
Awaiting for your reply.
Regards,
Archana Rao
Part Number: DAC0800 My question concerns the DAC0800 8 bit D/A converter.
I wish to use this part to drive a somewhat nonlinear resistance with controlled current in the 50 to 500 micro-amp (peak) range.
The load would be connected between the two…
Part Number: DAC0800 I've request some sample from the site, I added the items in the cart and the checkout is correctly 0€. But when I want to pay there is this message:
Your cart contains more items than is allowed. Please limit your cart to 0 items…
Part Number: DAC0802 Other Parts Discussed in Thread: DAC0800 Hi team,
Could you tell me the difference between DAC0802LC and DAC0800LC? I found nothing in datasheet. But the AN mentioned: 'Reference to the DAC0800 herein also includes the DAC0802,…