Part Number: DAC11001A Dear Sirs;
following is our circuit:
Where:
DAC11001A’s VCC=+12V,VSS=-12V
Grad_REF=4.942V
We measured U14(OPA4180IPW) every pin’s voltage as following:
Pin1=4.974V
Pin2=4.942V
Pin3=4.942V
Pin5=-4.930V
Pin6…
Part Number: DAC11001A Other Parts Discussed in Thread: OPA4180 Dear Sirs;
following is our circuit:
Where:
DAC11001A’s VCC=+12V,VSS=-12V
Grad_REF=4.942V
We measured U14(OPA4180IPW) every pin’s voltage as following:
Pin1=4.974V
Pin2=4…
Part Number: DAC11001A Tool/software:
I need to know that in the application note of dac11001a.
They calculated external voltage reference error using inital error, load regulation, temperature coefficents error, but i want to know that how to calculate…
Part Number: DAC11001A Other Parts Discussed in Thread: EK-TM4C1294XL Hi Team,
I would like to check with you about the DAC11001A EVM, since MSP430E401Y EVM is not available currently, do we have another way to connect the DAC11001A EVM and PC? Thanks…
Part Number: DAC11001A Tool/software: I find no reference for the duration of the DAC internal temperature calibration cycle.
The data sheet says I can poll a status bit via SPI, or use the ALARM pin to find out when it is done.
Both of these are…
Part Number: DAC11001A Other Parts Discussed in Thread: BP-DAC11001EVM , Tool/software: Hi,
I have used the DAC11001A in my design to realize high-precision output.My design is completely based on the "BP-DAC11001EVM" design.Actually,the output is not…
Part Number: DAC11001A Tool/software: Hi experts,
One question from customer side is that why we use nV/sqrt(Hz) as the unit of noise density?
Is there any special meaning?
Thanks!
BR
Jim
Part Number: DAC11001A
Hi all,
I am looking into the DAC11001A's output voltage settling time parameters. However, only the typical time is provided, and I was wondering if there is any data available for the min/max settlings times of the part…
Part Number: DAC11001A Team,
we found that ROFS and RCM (pin 10 and 11) pins are swapped on the EVM. If we copy EVM sch, will that work?
Thanks!
Xiaochen
Part Number: DAC11001A I would like to harvest some DAC11001A parts from an older rev board to use on an upcoming rev. I know this is not best practice and it is not guaranteed to work after, but can you provide a process that gives us the best likelihood…