Part Number: DAC11001A Other Parts Discussed in Thread: MSP432E401Y
I recently using DAC11001A+EXP432E401Y EVM for testing the DAC11001A performance.
The setting is as below,
VCC: 8.5v
VSS:-8.5V
VREF : 5.3V
VIO: 5.1V
VDD: 5.1V
short J25, Other…
Part Number: DAC11001A Hi,
we would like to use the DAC11001A (or B) in a project but could not find specific information on the behavior of the temperature calibration mode.
1. How long does the calibration normally take?
2. What happens with the output…
Part Number: DAC11001A I am currently using a DAC11001A in a design and one issue I'm finding is that the DAC outputs the voltage relative to code 00h at reset. In my design, this equates to -10V. I do not want to supply -10V to any of the load devices…
Part Number: DAC11001A Other Parts Discussed in Thread: OPA828 , , DAC11001B The slew rate seems to be dependent on slope direction, see screenshot. This is the DACs output buffered with an OPA828 (and another line driver). The initialization parameters…
Part Number: DAC11001A Hi,
My customer need assistance.
Here is the datasheet of DAC11001A:
https://www.ti.com/lit/ds/symlink/dac11001a.pdf
On page 3, there is the figure of pins. On page 46, there is the layout.
But Vcc and Vss pins are not at same position…
Part Number: DAC11001A Hi Team,
In the DAC11001A, what are the isolation metrics (V_rms) between DGND, AGND, and AGND_OUT? Is there an issue with configuring a system where these are kept as separate, isolated grounds?
Beat Regards, Tom Liu
Part Number: DAC11001A Other Parts Discussed in Thread: OPA189 , TINA-TI , OPA192 , OPA827 Hey everyone, For an SMU-like device that requires good DC precision and fast settling, I'm evaluating the DAC11001A from TI. I have a few questions after going through…
Part Number: DAC11001A Other Parts Discussed in Thread: DAC9881 , DAC1282 , DAC91001 Hi team,
I didn't see the INL of DAC1282, but I think DAC11001A would be much more precise in DC output. I would like to confirm if it is the most precise DAC, especially…
Part Number: DAC11001A Tool/software: Code Composer Studio I developed a PCB with DAC11001A but with my uC TM4C1294 I cannot load the data.
In what order should you put CLR / and LDAC with the SPI port.
cordially
Wiotte Fabrice My Programm : VREF + =+10V…
Part Number: DAC11001A Other Parts Discussed in Thread: OPA828 , OPA455 , OPA462 , OPA827 Dear Technical Support Team,
I'd like to make a analog output system with DAC11001A and Opeamp.
①
Is it possible to output ±15V with DAC11001A?
EVM has OPA828…