Hi,
Input capacitance is specified 3pF(max) on the datasheet.
Could you show me actual typical value and dispersion for our reference?
Best Regards,
Kuramochi
Other Parts Discussed in Thread: DAC124S085 Hi,
My customer is evaluating the DAC124S085 and occurred following problem.
The problem is that 1) output voltage is different setting and 2) update timming of output voltage is wrong.
Both problems are happened…
Hi,
Could you tell me whether a chip is tested on all specified condition or a part of condition about INL/DNL?
For example, DNL is tested on 2.7V~5.5V or the speculated worst voltage.
Regards,
Kuramochi
Hi Linh,
Unfortunately the DAC121S101 is the only space rated DAC we have and it does not come in a quad version. The DAC124S085 is a functionally similar device with 4 channels, but it has a commercial rating.
Best,
Katlynne Jones
Other Parts Discussed in Thread: DAC124S085 hi *,
i was wondering how to best model and quantify the noise of the DAC124S085.
i guess it's somehow composed of noise of the internal resistor network plus the noise of the output amplifier/buffer but i couldn…
Other Parts Discussed in Thread: DAC124S085 , DAC122S085 I really like the Online versions of the datasheets for your parts.
For example this page
http://www.ti.com/document-viewer/DAC124S085/datasheet/detailed_description#snas34814731
Do all products have…
Part Number: AM5718 Other Parts Discussed in Thread: DAC124S085 Tool/software: Linux Hi All,
We are configuring SPI as per shown below in dts.
&mcspi1 { status = "okay"; ti,pindir-d0-out-d1-in;
spidev@0{ compatible = "ti,dac124s085";…
Part Number: TLV9004 Other Parts Discussed in Thread: DAC124S085 , LM2776 , , OPA192
I'm using the TI DAC124S085 with a 3.3V supply as a 4-channel 12-bit DAC driving up to about 200mA total, operating at frequencies up to 10kHz. I want to operate a rail…
Part Number: LM3281 Other Parts Discussed in Thread: TPS65279 , DAC124S085 , TLV9004 , , TPS7A05
I have a high-power 6V-18V power source, and will be knocking it down to 5V with a TI TPS65279, which will introduce a ripple at 500kHz (which I will endeavor…