Part Number: DAC161P997 Other Parts Discussed in Thread: DAC161S997EVM , DAC161S997 Tool/software: Hi,
I am designing a universal analog output module,
a) 0-20 mA DC
b) 4-20 mA DC
c) 0-5 V DC
d) 0-10 V DC
While using DAC161P997, I am unable…
Part Number: DAC161P997 Other Parts Discussed in Thread: DAC161S997 If the commanded output current is increased above 23ma or so, the output drops to a value close to zero. Is there a similar component that doesn't do this? We change the scaling after…
Part Number: DAC161P997 Tool/software: Hi, I designed a PCB using this particular DAC.But unfortunately the loop is not working.
The DAC is responding to MCU commands and also giving status, in status it is showing loop error, and the DAC is also…
Part Number: DAC161P997 Hello Everyone.
A very good morning.
We are planning to use 4 DAC161P997 in a single board to provide accurate 4-20mA output. We will be happy to hear your inputs regarding whether we require 4 separate +24V Loop+ supply…
Part Number: DAC161P997
Hello,
I need help with DAC161P997 application:
When I measure the output with an amperimeter it's work well (4 ~20mA), but when I connect with a PLC analog input (120R impedance) DAC output drops to 3,6mA after reaches…
Part Number: DAC161P997 Hello Everyone.
A very good morning.
We are planning to use 4 DAC161P997 in a single boards to provide accurate 4-20mA output. We will be happy to hear your inputs regarding whether we require 4 separate +24V Loop+ supply…
Part Number: DAC161P997 Other Parts Discussed in Thread: XTR117 , DAC8775 , DAC80504
7024.DocScanner 10-Sep-2022 9-44 am.pdf
Hello Everyone.
A very good morning.
We are planning to use 4 DAC161P997 in a single board to provide accurate 4-20mA…
Part Number: DAC161P997 Hi Team,
I have two questions for BASE pin.
[Q1]
Could you please let us know a recommended part number of NPN transistor and parameter(for example, hfe=xx etc.)?
[Q2]
I understood that don’t need external resistor…
Part Number: DAC161P997 Hi Team,
Can you help with the issue below?
The customer acquired a DAC for activation with a 4 to 20mA output, as shown in the circuit image below.
We are using the DAC161P997 as a 4 to 20mA loop, the project is working…