Part Number: DAC161P997 Other Parts Discussed in Thread: DAC161S997
I have a converter which converts 24V(loop+) to 5v and a LDO which converts 5V to 3.3V. Something happens without a reason like letting output pin of DAC(loop-) float or connecting it…
Part Number: LAUNCHXL-CC1310 Other Parts Discussed in Thread: DAC161P997 , CC1310 ,
Hi everyone,
I am working with LAUNCHXL-CC1310 and trying to interface CC1310 with TI DAC161P997 on it to achieve Single-Wire communication between them. Is it possible…
Part Number: DAC161P997 Other Parts Discussed in Thread: DAC161S997 , Hi,
I have a application using photo couple to control output current:
MCU signal through photo couple control output current.
Is such a method feasible? Is there anything to pay attention…
Part Number: DAC161P997 If you have a DAC161P997 with no power on the isolated portion of the design, what sorts of protections would you recommend for the DIN/DBACK/ACKB pins if the microprocessor may still attempt to communicate? Diode clamps to VD…
Part Number: DAC161P997 Hello,
The datasheet for this part says the OUT pin is taken to its ERRB state when one of a few types of errors occurs, if the Threshold number of errors occurs in a row. If there are singular errors, for example with parity or…
Part Number: DAC161P997 Hi,
My customer used the solution as AD5700+DAC161P997, they found they can communication with 7 pcs DAC161P997 in the system. When the node add to 8, the DAC161P997 fail to communication. But in the standard of the HART, it need…
Part Number: DAC161P997 I can not connect via SWIF link in simplex mode stably, I've connected NC pin (11) to ground in pcb layout, can it cause problem?
Part Number: DAC161P997 We need help regarding DAC161P997, an oscillation wav eform (ringing) is observed in the loop output current.
An oscilloscope snapshot is attached. The DAC’s output is connected to GND via a 100Ohm resistor when the DAC is commanded…
Part Number: DAC161P997 Hi,
I have the Current loop transmitter DAC161P997 and I am able to communicate with it, I send data over the single wire communications and I receive an ack of the data or in this case the current that I want to output. How do…
Other Parts Discussed in Thread: DAC161P997 I would like to use DAC161P997 in the simplex mode with optoisolator. In the datasheet for simplex mode is mentioned only transformer case (fig.30 of the DAC161P997 datasheet)
Is the any drawback if I use only…