Part Number: DAC161S997EVM Hi Guys,
I am trying to download the DAC161S997EVM software and the link that is sent to my email with download link is not working. Surprisingly the Ti chat support lady was also not able to get it working so wanted to ask if…
Part Number: DAC161S997EVM Other Parts Discussed in Thread: DAC161S997 I have interfaced DAC161S997EVM with Cortex-M4 Micro-controller and able to communicate with DAC161S997 over SPI bus. I am able to set desired analog output between 4-20mA and also…
Part Number: DAC161S997EVM Hi I just received the development kit. Installed the software as administrator.
I receive the following error when trying to connect to the board:
The first dialog to select the COMPORT doesn't show the COMPORT that becomes…
Part Number: DAC161S997EVM Other Parts Discussed in Thread: DAC161S997 I just received a DAC161S997EVM and cannot locate the software. The ti.com/tool/DAC161S997EVM website shows it to be not available. Where can I find software for this module? Either…
Part Number: DAC161S997EVM Other Parts Discussed in Thread: DAC161S997 Hi I want develop a RS485-4_20mA interface with the DAC161S997EVM, but i can´t put a new current value in the output of DA161S997, but I suspect that i do not start properly the…
Part Number: DAC161S997EVM Other Parts Discussed in Thread: DAC161S997 Hello team,
I have got the following error message when starting the SW of 4-20 EVB:
What should I do? please advise back.
Thanks in advance and regards,
Shai
Part Number: DAC161S997EVM Other Parts Discussed in Thread: DAC8740H , DAC161S997
Dear sir,
I am using DAC161S997EVM for Hart Modem. But it does not connect USB port.
It means that this is usually due to a required driver not being installed on…
Part Number: DAC161S997EVM Other Parts Discussed in Thread: DAC161S997 Hi,
I'm trying to test the DAC161S997EVM through the accompanying LabView software. I'm trying to write a test value to the DAC board by selecting an output current in the DAC161S997…
Part Number: DAC161S997EVM Other Parts Discussed in Thread: DAC161S997 Hi,
I want to connect the DAC161S997 SPI of the EVM board with a different MCU (Arduino in this case).
The problem is that I can't find an access to the CSB pin of the DAC.
My question…