Hi Royce,
Sorry for the confusion. I was attempting to quote the DAC3154 datasheet, and meant to say that the Sync needed to be aligned to sample 0, but the data clock does not.
Also, could you share with me where you got the Data Clock, SYNC and Data…
Other Parts Discussed in Thread: DAC3151 , DAC3484 , DAC3154 Hi,
I need to connect DAC3151 output to IQ modulator with below specs:
Vcm= 0.5V
Vdifferential = 0.8Vp-p (full scale)
Ri= 3Kohm
Ci= 1pF
Can you please provide the interfacing circuit with 4th…
Other Parts Discussed in Thread: DAC3164 , DAC3283 , DAC3171 , DAC3174 , DAC3154 Hi team,
We're interested in using the DAC3164 in our design and had a couple questions:
Most FPGAs guarantee Vod (output differential) of 250 mV. Looking at the datasheet…
Hi
May I ask how much resolution will be improved by combining two DAC in below devices?
2 x DAC3154 (10 bit)
2 x DAC3164 (12 bit)
2 x DAC3174 (14 bit)
If two 10 bit DACs will make 16bit, like DAC5681 it will be great. But not likely using open loop, just…
Hi Cameron,
We have DACs up to 16-bits in resolution, but does your application require that? For the simple to use DACs, the DAC3152 and DAC3162 are the same, just two extra bits on the DAC3162. If you want 14-bits, take a look at DAC3174. The DAC3174…
Hi YZJ,
The example project copied above is a great starting point for the ADS4229 and the DAC3152. For the ADC side, the only change needed is changing from a 14-bit interface to 12-bits. For the DAC side you'll need to change to a 10-bit interface but…
Other Parts Discussed in Thread: DAC3164 From a customer:
"We would like a clarification regarding the DAC3164 which we are incorporating into one of our new designs. I understand that the SYNCP/SYNCN signal is to be used for multichip synchronization…