Other Parts Discussed in Thread: ADS62P28 , DAC3161 Hi,
My customer want to use DAC3161, but it's not in a traditional wireless communication application. they use the DAC and high speed amp to drive a cable and then use ADS62P28 to sample the signal at…
Other Parts Discussed in Thread: DAC3161 Dear sir/madam
I am trying to configure the dac3161 as follows, made the sdenb is zero during the instruction cycle(1 byte) and data transfer cycle(two bytes), once this serial data passed to the dac, made the sdenb…
Other Parts Discussed in Thread: DAC3161 Using a TI DAC3161 (or maybe 3171) in a new design. We noticed some discrepancies between the data sheet (SLAS959A) and the DAC31x1 EVM schematic (revision A, 17 Apr 2013):
1. Data sheet says pins 51-54, 63-64…
Sangeetha,
Sure, we can probably find a good interface solution to the F28335 device. What type of communication were you planning on using from the DAC3161? The options should be listed in its datasheet here: http://www.ti.com/lit/gpn/dac3161
Regards…
Part Number: DAC3174 Other Parts Discussed in Thread: DAC3164 , DAC3151 , DAC3171 , DAC3154 , , DAC3161 Hi,
In DA3174 datasheet (SLAS837B –APRIL 2013–REVISED JANUARY 2017)
Pins 63,62,52,51 are marked as NC in "Pin Functions" Table it is mentioned…
Part Number: DAC3161EVM Other Parts Discussed in Thread: DAC3161 We planned on using the DAC3161 and purchased the DAC3161 EVM to test out the part. After following the instructions shown in www.ti.com/.../sluuan8.pdf , we were able to connect to the EVM…
Part Number: ADS5463EVM Other Parts Discussed in Thread: DAC3161EVM , FMC-DAC-ADAPTER , DAC3161 , ADS5463 , CDCM7005 , DAC3162EVM What is needed to connect these 2 Evms without an fpga ?
I need to connect them as a proof of concept with a simple connector…
Other Parts Discussed in Thread: ADS6128 , DAC3161 , TLV0834 Hi,
My customer is using TLK3101. He is selecting ADC and DAC at previous and subsequent stage of TLK3101 now.
He selected ADS6128 and DAC3161. Can these IC use with TLK3101?
I think ADS6128/DAC3161…
Part Number: DAC3164 Other Parts Discussed in Thread: DAC3161 , DAC3174 .
Champs- got a customer who is bringing a board up and we have a few questions-
1. The config20 register allows setting allows the DAC output to be set to a static value. I expected…