Part Number: DAC3162 I would like to use the 1.2 V voltage reference of the DAC3162.
The VREF pin is labelled as "Factory use only" but can I use it externally ?
Also, does anyone know the maximum current it can source and sink ?
Thank you. …
Part Number: DAC3162EVM Other Parts Discussed in Thread: CDCP1803 , SN65LVDS100 , DAC3162 Dear All,
I have the DAC3162EVM and the Xilinx AC701 (Xilinx Artix7 FPGA Eval Board).
The FMC connector on the DAC3162EVM and the AC701 are perfectly compatible. So…
Other Parts Discussed in Thread: DAC3162 , DAC3152EVM we try to produce a 10 MHz sin wave with a sampling frequency 80 MHz, we generate that sin wave with 8 sample points. the analog output of DAC3162 seems as stepped as in the attachment, i think we should…
Other Parts Discussed in Thread: DAC3162 , DAC3162EVM I would like to generate two identical (or as identical as possible) signals out of DAC A and DAC B of the DAC3162, that is same amplitude, frequency and phase, so they are a replica of one another basically…
Other Parts Discussed in Thread: DAC3162 I have an application for the DAC3162 at a sampling frequency of 160Msps. However, I don't need to use both converters, just one.
Can I just leave the unused output NOT CONNECTED (NC), or does it need to be…
Part Number: DAC3162EVM Other Parts Discussed in Thread: DAC3162 Hi Team, seeking for assistance.
I tried to drive the DAC3162 with an FPGA @ 200MHz. The DAC input is switched from 0x000 to 0xFFF and vice versa at every clock edge to check the full resolution…
Marvin,
You can only test the DAC or ADC EVM one at a time, not both together. Can you try testing the DAC3162EVM and use the attached instructions? Just load the DAC3162.ini file instead of the DAC3152.ini. Let us know if this works.
There are currently…
Part Number: DAC3164 Other Parts Discussed in Thread: DAC3162 Hello team,
Is the 500MSPS for DAC3164 per channel? What is the max data clock rate?
The part seems to be interleaved so I would think each channel would be 250MSPS? Does the same go for DAC3162…
HI Jayant,
The FMA adapter card should work both DAC3164 and DAC3162EVMs. When we labeled pins on DAC3162 we skipped some of the pins.
Regards,
Neeraj Gill