Part Number: DAC3162EVM Other Parts Discussed in Thread: DAC3162 I am currently working on a waveform generation project using the DAC3162 and am encountering an issue with the output signal strength. I would appreciate your insights into my current hardware…
Part Number: DAC3162EVM Other Parts Discussed in Thread: DAC3162 Dear Customer Service,
I am writing to inquire about the configuration of my DAC31x2EVM. I am driving the DAC3162 using an FPGA via an FMC-DAC adapter and monitoring the output on an oscilloscope…
Part Number: DAC3162EVM Other Parts Discussed in Thread: DAC3162 Hi Team, seeking for assistance.
I tried to drive the DAC3162 with an FPGA @ 200MHz. The DAC input is switched from 0x000 to 0xFFF and vice versa at every clock edge to check the full…
Part Number: TSW1400EVM Other Parts Discussed in Thread: DAC3162EVM Hello Team,
My client thinks the EVM he bought has quality problems.
Clock lights are not on after TSW1400EVM is connected to DAC3162EVM, neither LED3 nor 4 are on, and the fan…
Part Number: DAC3162EVM Other Parts Discussed in Thread: CDCP1803 , SN65LVDS100 , DAC3162 Dear All,
I have the DAC3162EVM and the Xilinx AC701 (Xilinx Artix7 FPGA Eval Board).
The FMC connector on the DAC3162EVM and the AC701 are perfectly compatible…
Other Parts Discussed in Thread: DAC3162EVM Hi everyone,
to output a dc value on a DAC3162EVM, do you see any problem just putting in the R6, R15 and R17 resistors without removing the transformer? also can I still use the 25 ohm R7 in place even if…
Hi Richard,
Is it possible for me to get the FPGA source project that produces the current DAC_SAMPLE_WISE.rbf FW? I see some older posts when this was provided to users...hoping that's still the case. I'm pretty sure that the issue I'm seeing with…
Hi,
The physical design package zip file is available on the TI web page for the EVM at http://www.ti.com/tool/DAC3162EVM . In that file are the schematics and bill of materials spreadsheet for the design, as well as layout information. The front page…