Other Parts Discussed in Thread: CDCP1803 , DAC3162 My hardware setup is currently a Xilinx SP605 evaluation board to TI FMC-DAC Adapter Rev D to TI DAC 3162 EVM Rev B.
Goal is to create a clock from the SP605, output on J39 or J40 (these are SMA outputs…
Part Number: DAC3162 Other Parts Discussed in Thread: , SN65LVDS100 Tool/software: Hello
I'm designing a PCB board with an FMC interface, including a DAC3162. I'm using the DAC3162EVM and the FMC Adapter card as references in the design. This board…
Part Number: TSW1400EVM Hi Team,
Can you help troubleshoot the customer EVM issue below?
The customer tried the TSW1400EVM board to evaluate ADC3643EVM and DAC3162EVM boards. they believe that the problem is with the 1GB DDR module on the TSW1400EVM…
Part Number: DAC3162 Other Parts Discussed in Thread: , THS3217 , OPA694 Dear community,
I'm designing a board and i wanted to use the DAC3162 to generate a single ended output between 0V and 1V to feed into a 50Ohm load. I have never worked with…
Part Number: DAC3164EVM Kindly see the Schematics of the DAC3164EVM and FMC-DAC Adapter Card (Both are TI make).
Also, see the DAC3162EVM Schematics.
The Webpage of both the EVMs' (DAC3164EVM and the DAC3162EVM) say that they are compatible with…
Part Number: TSW1406EVM Dear community,
I've seen other question about asking the files for different EVM but they are all closed or they provide broken links to solutions.
We want to design a single board that combines TSW1405EVM, TSW1406EVM, ADS4229EVM…
Part Number: TSW1406EVM Hi support,
I'have got a TSW1406 and a DAC3152EVM board. I wanted to try the pattern generator but unfortunately, based on releases notes, the TSW1406 support only the DAC3162.
Unfortunately the DAC3162EVM was not available…
Jim,
The customer asked the following questions in response to your last question:
It seems customer is feeding Matlab code to DAC then to ADC. When he bypasses the DAC and ADC to check sanity, he directly feeds matlab code to his phase computation…
The FMC-DAC-ADAPTER should support the DAC3161EVM.
The description on the FMC-DAC-ADAPTER only lists the DAC3162EVM, but this is a 2 channel version of the same device (3161 is single channel)
The Zynq Ultrascale+ EVM will be a good choice if it has…