Can the EXTIO Pin be left unconnected if not used? Or must it be connected to GND through a 0.1uF capacitor.
Also, the datasheet does not have any recommendations as far as the bypass capacitor network is concerned, nor does it mention anything about capacitance…
Part Number: DAC3174 Other Parts Discussed in Thread: DAC3164 , DAC3151 , DAC3171 , DAC3154 , , DAC3161 Hi,
In DA3174 datasheet (SLAS837B –APRIL 2013–REVISED JANUARY 2017)
Pins 63,62,52,51 are marked as NC in "Pin Functions" Table it is mentioned…
HI Jayant,
The FMA adapter card should work both DAC3164 and DAC3162EVMs. When we labeled pins on DAC3162 we skipped some of the pins.
Regards,
Neeraj Gill
Part Number: DAC3161EVM Other Parts Discussed in Thread: DAC3161 , DAC3164 I am going to interface DAC3161 EVM with Artix7.
1. Can i use JESD204 interface instead of LVDS interface?
2. If its not possible whether we have to design LVDS in fpga?
3. Presently…
Hi,
We are looking for the source code repository at this time for you. May we have an email address to send it to when we locate it?
We will also look to see what hooks may have been included in the current firmware for timing, if any. If provision…
Hi
May I ask how much resolution will be improved by combining two DAC in below devices?
2 x DAC3154 (10 bit)
2 x DAC3164 (12 bit)
2 x DAC3174 (14 bit)
If two 10 bit DACs will make 16bit, like DAC5681 it will be great. But not likely using open loop, just…
Hi Matt,
One more follow up question on DAC3162 (and it's EVM). This relates to whether an in-line choke (inductor) can be used which I think would also improve the common-mode performance. I noted that on the reference board designs the current-source…