Part Number: ADS4149EVM Other Parts Discussed in Thread: DAC3283EVM , , THS4509 , DAC3283
Hi,
I want to make loopback environment of DAC3283EVM & ADS4149EVM for test.
So, I will revise DAC3283EVM and ADS4149EVM.
R1 & R3 resistive network will use 25…
Part Number: DAC3283EVM-SW Other Parts Discussed in Thread: DAC3283EVM , DAC3283 Dear sirs,
We use DAC3283EVM board in our testbench. DAC_GUI tool proposed by TI is quite handsome and useful.It allows to save/restore configuration in/from txt file.
But…
Ok, so I loaded your latest register values and enabled the FIFO. The distortion should disappear when you disable the Clock Divider Sync. This should only be enabled at startup and then disabled, or just disable it completely. Try that and let me know…
Part Number: DAC3283EVM Are there any limitations for a low output DACCLK frequency? There isn't a low-end frequency specification but the characteristic data only goes down to 50MHz in figures 21-24 of the datasheet. We have an application where the…
Part Number: DAC3283EVM Other Parts Discussed in Thread: DAC3283 We are planning to use a single SN65LVET22 (Vcc @ 3.3V) to provide inputs to the DACCLK & OSTR inputs of the DAC3283 with the circuit shown in figure 45 of the DAC datasheet. Are there any…
Other Parts Discussed in Thread: DAC3282EVM , DAC3283EVM , DAC3283 Hi,
I would like to do measurements based on the WiFi 802.11ac standard which requires a carrier frequency in the 5GHz band and a signal bandwidth of 80MHz.
Is it possible to generate such…
Other Parts Discussed in Thread: DAC3283EVM , CDCE62005 , DAC3283 Hi,
We have just purchased the DAC3283EVM eval board. Our application requires us to interface to the USB and configure the eval board by command line and therefore we cannot use the PC GUI…
Other Parts Discussed in Thread: DAC3283 All,
I have a customer that is trying to install the SW for this card and it halts at the NI installation with an error :
+++++++++++++++++++
"The NI LabVIEW Real-Time FIFO for Runtime installation failed with…
Other Parts Discussed in Thread: DAC3283EVM I purchased a TSW3100 pattern generator with DAC3283EVM evaluation board kit from Mouser but the operating software for the TSW3100 is an old version. According to the installation instructions I need version…
Other Parts Discussed in Thread: DAC3283EVM , DAC3283 Hi,
I was wondering if anyone had some sample Matlab code for generating the vectors that go into the TSW3100 which will be used to generate RF using the DAC3283EVM. Long term, I am planning on trying…