Part Number: DAC34SH84EVM Other Parts Discussed in Thread: DAC34SH84 , , DAC5675A-SP Hi All,
For one of my designs I need to generate two independent DAC output voltages (with few discrete steps only) @ 400 MHz and above. Both the outputs should change…
Part Number: DAC34SH84EVM Hej,
I am getting stuck in interfacing my Kintex 7 board FPGA to 34SH84EVM. Do I have to follow this way as below by sending 3 signals including: DATACLK, DATA and SYNC?
Is there anybody using FPGA instead of using pattern generators…
Part Number: DAC34SH84EVM Other Parts Discussed in Thread: DAC34SH84 , FMC-DAC-ADAPTER Hej,
Is there anybody having the same problem with physical connection of the DAC34SH84? The yellow locking part doesn't fit to both holes of the adapter.
Thank you…
Part Number: DAC34SH84EVM Other Parts Discussed in Thread: DAC34SH84 , FMC-DAC-ADAPTER Hej all,
I am using DAC34SH84EVM rev D (which I guess it is reference D) and FMC-DAC adapter rev D. I did cut off the tab to make them being able to connect.
Now I have…
Part Number: DAC34SH84EVM I connect the DAC34SH84EVM with the Xilinx FPGA board VC707 via the FMC-DAC adapter. At this point, I would like to produce some signal with low frequency from the four channel, so I remove T1 T2 T3 T4, T8 T9 T10 T11. In addition…
Part Number: DAC34SH84EVM Hi,
we are using a DAC34SH84EVM in order to generate constant output levels that change every 200us. We provide data and CLK through the FMC adapter connected to a SPARTAN FPGA. We managed to make it work pretty fine with the…
Other Parts Discussed in Thread: DAC34H84 , DAC34SH84 , CDCM7005 , CDCE62005 I was following the steps in DAC348x EVM manual: http://www.ti.com/lit/ug/slau432/slau432.pdf testing with TSM1400. The DAC I am using is DAC34SH84 EVM and at 3.4 DAC348x Example Setup…
Other Parts Discussed in Thread: DAC34SH84 Hello everybody,
I'm configuring the DAC34SH84 evaluationboard with the GUI and I wonder how to save the configuration to the DAC, so that it knows what to do after switching off and on again. I also recognised…
Other Parts Discussed in Thread: FMC-DAC-ADAPTER , DAC34SH84EVM I've got a DAC34SH84EVM Rev. D and a FMC-DAC-Adapter Rev. D which I'd like to connect.
On both sides of the socket on the DAC-Board there is a metal pin, that doesn't fit through the…