Part Number: TI-JESD204-IP Other Parts Discussed in Thread: DAC37J82EVM , DAC37J82 , Hi TI team,
I got two EVMs on the hand TSW14J56+DAC37J82. According to the DAC37J82EVM user guide, I can make the quick-start prodedure succesfully.
We use LMF=222 configuration…
Part Number: ADS54J20 Other Parts Discussed in Thread: DAC37J82 , , LMK04828 Hi! We have a new project where we want to connect two ADCs and a DAC via JESD204B with a Xilinx Ultrascale+ XCZU4CG. I read several information about JESD204B already, but I have…
Guy,
I am guessing the issue is a Link Configuration error. I would try setting 0x51 to 0xDD then 0xDE to verify there are no disparity or not-in-table code errors.
I have seen in the past where a FPGA entry for an ILAS parameter is defined different…
Part Number: DAC37J82EVM Hi,
At the evaluation board :DAC3XJ8XEVM, we removed the transformer and try to use the single ended output.
However, noticed that there is a DC offset at the AOUTP and AOUTN.
can you please help where I can adjust the DC offset…
Part Number: DAC37J82 Hi team,
A question from one of our customers, could you make any troubleshooting suggestions?
In the same configuration, the output power of a 5M 50M 100M single tone on the spectrometer decreases with frequency, but peak detection…
Part Number: DAC37J82 In order to use the device ( DAC37J82) I need to use dual channels for two independent dataflows with the same rates.
For example to use 1\2\4 GT lanes lanes for one dataflow, and another 1\2\4 GT lanes for the other dataflow.
However…
Part Number: DAC37J82 The DC power quoted in para 6.5 - is this for a single channel or both channels? I will operate close to mode 7 - dataSheet page 9; 625MSMPS, PLL OFF, NCO OFF etc. Both channels will output a 190+/-50M wide signal. from independent…
Part Number: DAC37J82 Hi team,
1、One of our customers has the following questions, could you help me reply
We need register values that match our setting .
The settings for using the DAC37J82 are shown below.
Input Clock : 500Mhz
Input Data rate : 500MS…
Part Number: DAC37J82 Other Parts Discussed in Thread: DAC38J82 Table 47 on Page 69 of the datasheet shows the following register configuration for register 16:
The datasheet says:
The QMC correction phase term for the DACAB path. The range is –0.5 to…