Part Number: DAC37J84EVM Other Parts Discussed in Thread: DAC37J84 , Tool/software: I hope this email finds you well. I am working on a custom project that involves interfacing the DAC37J84 IC via SPI using an FT4232H chip. While attempting to utilize…
Part Number: DAC37J84EVM Other Parts Discussed in Thread: TSW14J58EVM , TSW14J59EVM , , DAC37J84 , TSW14J57EVM , TI-JESD204-IP Tool/software: Hi Dear,
Does TSW14J58EVM and/or TSW14J59EVM support DAC37J84EVM?
Regards
Erivelton Castro
Part Number: TSW14J59EVM Other Parts Discussed in Thread: ADS54J60EVM , , DAC37J84EVM Tool/software: Hi,
I created the lab with TSW14J59EVM with ADS54J60EVM and DAC37J84EVM, but the HSDC Pro does not have support for these plataform.
Does TSW14J59EVM…
Part Number: DAC37J84EVM Tool/software: Hi Dear,
I am going to work the ZCU102 with this DAC37J84EVM.
Can you help giving me a reference design for quick start?
Regards,
Erivelton Castro
Part Number: DAC37J84EVM Other Parts Discussed in Thread: DAC37J84 Tool/software: Hi Dear,
Will I need to TSW14J10 interface board to work with the DAC37J84EVM connected on ZCU102?
Regards,
Erivelton Castro
Part Number: DAC37J84EVM Tool/software: RF output goes into 75ohm transformer with 2:1 impedance ratio (minicircuits JTX-2-10TA+)
The 2:1 impedance ratio is 100ohms differential on balanced side connected to DAC (which is correct) and 50 ohms on side…
Part Number: DAC37J84EVM Tool/software: Hi Dear!
I have the Xilinx ZCU102 evaluation board. I am using this FPGA board with DAC37J84EVM.
Can I use the High Speed Data Converter Pro GUI (HSDC Pro GUI) with this ZCU102 MPSoC Ultrascale+ FPGA EVM …
Part Number: DAC37J84EVM Other Parts Discussed in Thread: DAC37J84 Hi,
I will use ZCU102 evaluation board with DAC37J84. I intend to use the ip core JESD204 from the xilinx vivado software. Can I use IP Core JESD204B from the supplier xilinx and not…
Part Number: DAC37J84EVM Other Parts Discussed in Thread: LMK04828 , DAC37J84 Hi, Support
I'm referencing to the TI EVM board: DAC3XJ8X EVM for one of our design.
Regarding the VCXO, is there a special requirement for it??
The VCXO phase jitter…
Part Number: DAC37J84EVM Other Parts Discussed in Thread: DAC37J84 Hi,
I am a beginner in FPGA design.
I would like to generate sine and cosine waves using DAC37J84EVM and Xilinx FPGA part no: Kintex-7 KC705.
I created the sine and cosine wave samples…