Part Number: DAC38J82 Hello,
I am reading the reference design(zc706_8b10b) about TI_204c_IP.
I have a question about sysref.
In TI_204c_IP_ref.sv, I see the Sysref signals tied to '0', like below.
So why do like this in reference design?
…
User,
You sent a config file from the DAC38RR82 but above the post calls out the DAC38J82. Attached is a config file for the DAC38J82 with your settings. Give this a try.
The serdes pll is running at 3GHz, with the MPY set to 20 and the PLL reference…
Part Number: DAC38J82 Dear TI members,
I had met a very strange phenomenon while using the DAC38J82IAAV on my design. There is 4pcs DAC38J82 IC on one board with 8 output port. After initial check, i found the ports can't output sine signal waveform…
Part Number: DAC38J82 Hello TI,
in our custom circuit we have a DAC38J82 with DACA and DACD connected to SMA connectors (differential-single ended conversion).
When I enable the DAC output with the sif_txenable bit in the config3 register or externally…
Part Number: DAC38J82 Hi,
We have planned to use the DAC38J82 to generate output frequency range of 200MHz to 700MHz.
Our front end return loss requirement is greater than 17dB we simulated the analog front end of your evaluation board and the results…
Part Number: DAC38J82 HI!
I am planning to use DAC38J82 for the below application and i have the below query,
Application:
DAC CLK: 2400MHz
Output Freq: 250 to 700 MHz
Resolution: 16Bit
Fdata: 600Msps
Query:
1)I have only CML clock outputs…
Part Number: DAC38J82 Hello All,
I'm working with DAC38J82 in a customised hardware. I'm having an issue in getting the DAC output. Here is my configuration.
DAC input clock is 2457.6MHz. DAC PLL is not used. No SYSREF input.
I'm trying to use the…
Part Number: DAC38J82 Hi team,
The DAC works without the internal phase-locked loop. The sample clock cannot be generated using the internal PLL, read config108 0x0003. Input clock is 250M and it's required to generate 1GHz sampling clock.
The following…
Part Number: DAC38J82
HI!
I am planning to use DAC38J82 for below application,
DAC output Signal =275MHz to 675MHz
NCO Freq=475MHz
Throughput for complex data with interpolation =600MSPS(480MHz Signal BW)
Interpolation=4
Sampling Freq: 2400…