Part Number: DAC38J84 Other Parts Discussed in Thread: DAC38J82 , Hi everyone,
I have used DAC DAC38J82 for generating only one Output with Output Frequency upto 700 MHz by using following configuration LMF = 421 Sampling frequency : 2.4576GHz Now I am planning…
Part Number: DAC38J84 Hello,
Looking at the 0x6C register, I see that there is the "alarm_sysref_sh". The GUI states that :
But in the datasheet, it is marked as reserved :
Is this a 'functioning' alarm? If so, what are CDRV_SER, OSTROBE,…
Part Number: DAC38J84 Other Parts Discussed in Thread: LMK04828 hello, jim
My custom board can work normal when setting as follows
Fdata = 300M
LMF =442
interpolation = 4
Fdac = 1200M
SerDes Linerate = 6000M
but when I double the interpolation to 8…
Part Number: DAC38J84
I am working with DAC38J84 in NCO mode in the following way:
1. set a new frequency through SPI (registers 0x14 - 0x16)
2. using a one sysref pulse to update the NCO ( 0x1E = 2222 , 0x1F = 2220)
DAC_CLOCK = 1920MHz
SYSREF WIDTH = 5…
Part Number: DAC38J84 Other Parts Discussed in Thread: DAC38J82 Hi sir,
A customer have some query regards DAC38J84.
He want to configure DAC in that his target was NCO+External DATA is his final output. He is able to do configure NCO and he got output…
Part Number: DAC38J84 Dear Sir/Madam,
I am using a DAC IC:( DAC38J84) in which I require the output impedance at the frequency 40+/- 3 MHz.
Regards,
Vigneshwar Raj
Part Number: DAC38J84 I configured the VC707 and DAC38J84, and the indicator light showed that they were properly configured. I followed the Quick Start Page of DAC38J84EVM without tuning the other control buttons in DAC38J84EVM.
I connected the SMA output…
Hi,
I see you have opened a new thread. We can use this new thread to discuss. I have forwarded to appropriate folks to answer. Thanks.
https://e2e.ti.com/support/data-converters/f/data-converters-forum/984649/dac38j84evm-dac38j84---sfdr-out-of-speci…