Cameron,
It seems the new EVM has solved the connection issues and is allowing you to communicate properly, that is good to hear. This procedure should be all that is needed, no un-mentioned steps were left out as I just tested on an EVM in the lab.
…
Part Number: DAC38J84EVM Now that we have the NCO mode working nicely using the on-board VCXO, PLL and clock distribution, we wish to substitute an external CLK to the CLKIN J17 of the DAC38J84EVM. We obviously need to make some changes on the GUI Quick…
Part Number: DAC38J84EVM Hi Team,
I want to use DAC38J84EVM with TSW15J56 to evaluate customer's requirement, but have some trouble in setting the configuration. Could you pleas help with it.
Customer requirement is:
204B parameters: L/M/F/S=8/4/1…
Part Number: DAC38J84EVM Other Parts Discussed in Thread: DAC38J84
Hello,
I'm measuring the SNR of the DAC38j84 by applying a single tone (const=0x0000, fout=400MHz) at the input with NCO (on the evaluation board with GUI evaluation software).
Settings…
Part Number: DAC38J84EVM Other Parts Discussed in Thread: DAC38J84 , LMK04828 Hi.
What is the current consumption of DAC38J84 EVM.
I am using a power adaptor of 5V and 2A..but JESD linkup is not happening.
At full operation ( when JESD interface is up)…
Part Number: DAC38J84EVM Other Parts Discussed in Thread: LMK04828
Hi,
I have problems with DAC3XJ8X GUI. I installed V1.3 and there is always an error displayed see attached. I couldn't find the problem and the evaluation board sometimes works and sometimes…
Part Number: DAC38J84EVM Other Parts Discussed in Thread: DAC38J84 , LMK04828 Hi
I am using DAC38J84 EVM.
In the Datasheet, it is mentioned that Clock and Sysref Standard is LVPECL (AC Coupled).
But in the EVM Schematics, Sysref is DC Coupled . So rec…
Part Number: DAC38J84EVM Other Parts Discussed in Thread: DAC38J84
I'm designing my third-party FPGA( XILINX KCU040 kintex ultrascale ) evaluation board with a standard FMC-HPC connector to DAC38J84EVM. All jumpers at DAC38J84EVM are left untouched…
Part Number: DAC38J84EVM Other Parts Discussed in Thread: TI-JESD204-IP , LMK04828 Dear Ti.
I'm using xilinx FPGA kcu040 kintex ultrascale trying to drive the DAC38J84EVM, all pins should have been assigned properly.
I have tried both TI-JESD204-IP…
Part Number: DAC38J84EVM Other Parts Discussed in Thread: DAC38J84 Hello,
The data lines from FMC to the DAC are jumbled up. For example, DP5_C2M from FMC is connected to RX7. It is true for other data lines also. Why is it connected this way? Please forgive…