Part Number: DAC38J84EVM Other Parts Discussed in Thread: DAC38J84 DEAR TI,
I am using a third party alinx xczu9eg ultrascale+mpsoc development board for JESD204B based DA development(DAC38J84EVM), The FMC daughter board I am using is DAC38J84EVM , where…
Part Number: DAC38J84EVM I'm designing my third-party FPGA( XILINX Zynq UltraScale+ XCZU9EG MPSoC ) evaluation board with a standard FMC-HPC connector,which is not in the support list of HSDC pro software.
My question is following:
1.weather and…
Part Number: DAC38J84EVM Other Parts Discussed in Thread: LMK04828 , DAC38J84 Hi,
I am use a sys_sync signal to enable the DAC output. After the rising edge of sys_sync signal reach to the SYNC of LMK04828, there are outputs on the SDCLKout*.
I can capture…
Part Number: DAC38J84EVM Other Parts Discussed in Thread: DAC38J84 Hi,
I am using the DAC38J84 on the EVM with an Arria10 dev board and for now, the JESD part works fine. However I am facing a problem using the NCO on this DAC. For my project, I plan to…
Part Number: DAC38J84EVM I enable the NOC function, set the Coarse DAC Gain to 10, the mixer gain disabled, I get 0.95V Vp-p, is it right? How can I get 1.5V Vp-p? Thanks!
Part Number: DAC38J84EVM In pll disable mode, the DACCLK is used straight from the pin and SYSREF needs to respect the setup and hold times.
On the eval board, the LMK can generate up to 2.457GHz for the device clock with the divider set to 0. However…
Part Number: DAC38J84EVM Other Parts Discussed in Thread: DAC38J84 , , LMK04828 I purchased DAC38J84EVM and connected it to the VC707.First, I downloaded the configured JESD204 to VC707.In accordance with the requirements in the manual, I programmed DAC38J84…
Part Number: DAC38J84EVM Other Parts Discussed in Thread: LMK04832 , LMK04828 Dear sirs, I have copied the screens as shown on the GUI with the manual settings as we would like to work with. Is it possible to receive from you the corrections for that set…
Part Number: DAC38J84EVM Other Parts Discussed in Thread: DAC38J84
Tool/software: WEBENCH® Design Tools
Hi sir,
We are using DAC38J84EVM with the help of DAC GUI
I tried giving a TEST FILE in that Single tone of 25MHz is used in HSDC Pro with that…
Part Number: DAC38J84EVM Other Parts Discussed in Thread: DAC38J84 Dear,
I bought the dac38J84_evm board to bench my project.
But the SFDR is very bad -48dBc (hd2)
Setting :
JESD204B - 6.144Gbps
Sample rate 614.4 MSPS (FPGA)
Interpolation : 2
DAC sample…