Part Number: DAC38RF85 Hello.
In register 0x"43E" fild BUSWIDTH default value is 010. Description incomprehensible for me.
Selects the parallel interface width (16 or 20 bits). 0 : 20 bits 1: 16 bits
I use Xilinx JESD204Phy IP. This core use 8/10…
Part Number: DAC38RF85 Hello.
Instead TCM3-452X-1+, I have to use TCM2-43X+. I added 560 nH termination inductors to 1.8V in DAC output. Now, i see single tone, and 1.8V common mode.
What other changes do I need to make to the termination scheme?…
Part Number: DAC38RF85 Hello.
On my board, I follow the instructions to get single tone output.
I adjust VCO frequency and VCO_LF voltage chenges to 3. I see that PLL is look.
But in output of DAC, negative voltage constant ~ -1V.
Then i set SPI…
Part Number: DAC38RF85 Hello.
I need generate signal with 600 MHz bandwidth, in the 1.2GHz carrier friquency.
If I understand correctly, i need genegate quadrature signal in zero carrier frequency, with sample frequency 600MHz. In the DUC, need set…
Part Number: DAC38RF85 Section 8.3.1 of the datasheet ( bottom of page 39 ) references a LOOPBACK setting in SRDS_CFG1 register.
The section (8.5.86) describing the SRDS_CFG1 register has no LOOPBACK setting.
What is the loopback function and how…
Part Number: DAC38RF85 Hopefully a v simple question here !
The datasheet indicates that the PAGE_SET register is valid when PAGE_SET[2:0] is 000.
Surely this is not correct, as once the register has been changed to select another page, you will never…
Part Number: DAC38RF85 I am not getting consistent data read from the TEMP_PLLVOLT register between resets of the device.
All other registers seem to behave OK.
Sometimes after reset I am seeing negative values returned in the temperature (0xEAE2…
Part Number: DAC38RF85 Is there any data available regarding the startup time for this device ?
How long after device reset before the SPI interface is usable ?
How long after device reset before the AUTOLOAD_DONE bit is asserted ?
Part Number: DAC38RF85 The datasheet has the following data for the BUSWIDTH field in register SRDS_CFG2:
Bit: 4:2
Type: R/W
Reset: 010
Description: Selects the parallel interface width ( 16 or 20 bits). 0: 20 bits 1: 16 bits
Is this decode…
Part Number: DAC38RF85 The Register Maps section of the datasheet appears to contain 3 different sets of reset values for each register.
There is a reset value in the section header for each register.
There is a "value after reset" for each bit…