Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed from November 25 through December 2. Thank you for your patience.
Part Number: DAC39RF10EVM Hi,
I would like generate 1ns pulse width of a pulse generation using DAC39RF10EVM. Could you show a screen shot of the pulse, rise time and fall time of the generated pulse?
Thank you,
Sujatha
Part Number: DAC39RF10EVM Other Parts Discussed in Thread: DAC39RF10 Hi team,
Here is a question one of our customers is experiencing, could you please provide some troubleshooting suggestions?
After the GUI is installed, an error is reported every time…
Part Number: DAC39RF10EVM The DAC on this board has VDDIO set to 1.8V and the input specs on SCS input pin (connected to net named DAC_CS_n) is VDDIO + 0.3V = 2.1V.
If R163 which pulls up to 3.3V at U36's input damage or stress the DAC as the pulled up…
Hi Siyuan,
There may be a way to generate short pulses by inputting two pulses into the LMG1020, one on IN+ and another identical pulse with a 500ps delay (or whatever your desired pulse is) on IN-. Please refer to section 8.2.2.2 and figure 10 on the…
Part Number: DAC39RF10EVM Hello, My customer would like to use “EXT->DACCLK | LMK-> FPGA Clocking Option”. The EVM users guide suggests the following modifications. - Remove C141 and C142, populate C136 and C139 - Remove C138 and C140…
Part Number: DAC39RF10EVM Hi team
Could you tell the role of C252, C253 and C254 used in the EVM? These are for bypass cacitors or EMI filters or other roles?
Regards,
Noriyuki Takahashi
Part Number: DAC39RF10EVM Other Parts Discussed in Thread: TPSM82913 Hi team,
There are some questions in order to undestand the EVM schematic and use the schematic as reference for the designing.
Q1. Could you tell the meaning of "3A, Vin = 3V → 17V…
Hi Matt.
I recently (yesterday) confirmed that my EVM links to JMODE5 and 8B/10B (both subclass 1 and subclass 0).
(Please understand that photos cannot be uploaded due to company regulations.)
However, upon further testing, I found that the input signal…
Part Number: DAC39RF10EVM Other Parts Discussed in Thread: TSW14J59EVM , What pattern generator would I use for the DAC39RF10EVM? The TSW14J59EVM does not seem to be available as I have already contacted the Support Center.