Part Number: DAC43401-Q1 Hi, Team
One of my key customers is asking a technical question regarding the relationship between VDD and OUTPUT voltage on the DAC43401-Q1.
If reference is tied to VDD, and VDD can vary between 4.9V, 5.0V, and 5.1V, how…
Part Number: DAC43401-Q1 Other Parts Discussed in Thread: TPLD2001 I wanted to reach out regarding a component I am interested in using: DAC43401-Q1. I was hoping to use this component for I2C controlled PWM generation at 25KHz but the datasheet doesn…
Part Number: DAC43401 Tool/software: Hello,
the datasheet of the DAC43401 lacks specifications for the digital I/Os:
- output low voltage (SDA)
- leakage currents (SDA,SCL)
If I understand the recommended operating conditions (Vih min 1.65V) correctly…
Part Number: DAC43401 Hi team,
My customer need a PWM signal which has 100us +/-5% of cycle period and 5us +/-5% of pulse width.
What is the accuracy for DAC43401's CWG? Is there a Smart DAC device that can achieve above requirement?
Best Regards…
Part Number: DAC43401-Q1 Other Parts Discussed in Thread: DAC43401 My chip has 0x48 slave address and NVM has some settings so I reset settings right after booting.
I don't use any PMbus function.
Chip VDD input is 5V and I want to make sqaure wave…
Part Number: DAC43401 Hello Team,
Can you help on the following customer request.
We are considering to use in one of our new devices DAC43401DSGR as adjustable/programmable voltage reference. Usage explanation: 1. Our new design won't have MCU…
Part Number: DAC43401-Q1 We are using VDD 5v for the ref vdd and we want to produce square wave (0 ~ 1.8v)
Now I'm initialzing
0x25, 0x0170
0x26, 0x0000
0xD1, 0xC000
0xD3, 0x0108
0xD3, 0x0118
But, it's not working.
Please check for initializing…
Part Number: DAC43401-Q1 My device found 2 slave addresses for DAC chip. (Address 47 & 48)
Which is the right one? and why 2 slave addresses are appeared?
Part Number: DAC43401-Q1 Other Parts Discussed in Thread: DAC53701 , DAC53701EVM GENERAL_CONFIG Register Field Descriptions
Want 0~1.8v square wave output, need to explain I2C setting method
Part Number: DAC43401-Q1 Tool/software: Please review my answer.....
I tested slew_rate change and there's no response.
I tested 2 days ago changing SLEW_RATE from 0000 to 1111 and there's no change.
test environment is repeating below chunk…