Part Number: DAC43608 Hi there,
My customer needs to turn off the output of DAC43608, and he is considering setting /CLR low to do this.
I noticed that /CLR only clears the buffers and active registers, so I would like to confirm if /CLR can turn off…
Part Number: DAC43608 Hi there,
My customer is evaluating DAC43608. He has a question about the address byte.
The address byte should be 8-bit. But Table 1 shows that Address byte is DB [32:24], which is 9-bit, is this a typo?
And could you provide example…
Part Number: DAC43608 Hi expert,
This session is related question from the following session.
http://e2e.ti.com/support/data-converters/f/73/p/857205/3172342#3172342
(your comment)
If there is a fault on the I2C line, writing a single byte over I2C…
Part Number: DAC43608 Hi team,
Datasheet mentions A0 can be tied to VDD. It doesn't require pull up resistor, right? Is it just CMOS input? Just want to make sure just in case.
When some of DAC43608 VOUT is unused, is it OK to leave it open?
Regards…
Part Number: DAC43608 Hello team,
Could you please let me know the design procedure for resistor voltage divider output?
The customer is trying to connect DAC43608 VOUT to motor driver VREF via voltage divider.
VREF will have a filtering capacitor to…
Part Number: DAC43608 Other Parts Discussed in Thread: DRV8874 Hello team,
My customer is considering to connect DAC43608 to motor driver (DAC8874, etc) VREF.
Is it OK to connect DAC43608 output to DRV8874 directly?
DRV8874 D/S doesn't show VREF input…
Part Number: DAC43608 Hello Guys,
Good day.
Our customer wants to know the minimum and maximum values of the Reference Input Impedance of DAC43608 when all channels are powered on since only the typical value of 12.5Kohms was specified on the datasheet…
Part Number: DAC43608 Hi,
Customer have an issue about read back NG after SW_RST.
Sequence is below,
- Assert SW_RST
- Wait time 15ms
- Read DEVICE_ID : confirmed 010100b
- Write 0x00 to PDNn(n=0~7)
- Read PDNn(n=0~7)
- Read Result : 0xFF (Readback…
Part Number: DAC43608 Other Parts Discussed in Thread: DAC60508 Hi all,
My customer want to use 8 ch dac as 8 reference voltage outputs (below 1v). Can I know the output current ability in each channel? If I need 20mA / ch, can I use dac43608 or any…
Part Number: DAC43608 Hi Expert,
My customer have an issue about no output when the Vcc ramp up speed is fast. (POR is abnormal condition???)
They set output voltage registers by I2C. Then, they confirm to receive ALK signal. (They think, I2C communication…