Part Number: DAC5311 Other Parts Discussed in Thread: LMR14203
I am designing a power supply for a product that uses the DAC5311.
The power supply uses a switching power supply LMR14203 for efficiency.
The drive voltage of the DAC5311 in normal…
Part Number: DAC5311 Other Parts Discussed in Thread: DAC7311 Hello
I am using DAC5311/DAC7311 in our design , when I connect it to load the output is 0, without load the output is ok.
What can be the problem?
Part Number: DAC5311 Hi TI Team,
Thank you for your support. One of our customers asking,
*Which way is the Pin 1 for DAC5311IDCKT?
Reason is Datasheet show Pin 1.
2.0V to 5.5V, 80μA, 8-, 10-, and 12-Bit, Low-Power, Single-Channel, DACs…
Part Number: DAC5311-Q1 Other Parts Discussed in Thread: DAC5311 , DAC088S085 , TLV5632 Dear TI design support,
I am searching a DAC to generate a number of voltage levels in the range 0V-1.5V. I came across DACs offered by TI. For instance DAC5311…
Part Number: DAC5311 Hi Sir,
DAC5311 interface is I/F, not I2S. What is its digital I/F?
Do you have its programming code (C language) can provide to us for customer request?
Thanks, Ian.
Part Number: DAC5311-Q1 Other Parts Discussed in Thread: DAC5311 Hi experts,
the DAC5311-Q1 datasheet define the VinH limit of AVDD=5V and AVDD=1.8V, but not define when the AVDD=3.3V. can you tell me this limitation on AVDD=3.3V?
customer want…
Part Number: DAC5311-Q1 Other Parts Discussed in Thread: DAC5311 , DAC53204 , DAC53701 , DAC53401 Hello Team,
I would like to confirm if the minimum supply voltage of 1.8V is accurate for the DAC5311-Q1? I checked that the catalog version DAC5311 rated…
Part Number: DAC5311 Dear Expert
1. Ch 1 CS Pin ,Ch2 Clock ,Ch3 Input
2. Ch 1 CS Pin ,Ch2 Clock ,Ch3 output
3.Bode diagram
4. Schemetic
Now we have question is this chip, input normal, output have two problems, one is jitter, the…
Part Number: DAC5311
Hello Ryan Andrews,
1. How to configure DAC5311 with ARDUINO UNO?
2. What are the steps need to be followed?
3. Please share DAC5311 firmware with any microcontroller, if you have
So that I'll get a basic idea.