Part Number: DAC53202 Hello team,
The VREF pin says "This pin must not ramp up before VDD.".
Are there specific orders for this timing? (ex. msec, nsec)
Best, Taketo
Part Number: DAC53202 Tool/software: Hello.
I would like to know about the functions of the DAC53202. I am currently experiencing a problem with a product that uses the DAC53202. It seems that noise is being mixed into the DAC53202's I2C signal, causing…
Part Number: DAC53202 Hello, I intend to use DAC53202 with Internal Reference. As per my understanding the connection of VREF pin should be just a bypass cap when using Internal Reference.
Datasheet mentions to add a pull up to VDD when External Reference…
Part Number: DAC53202 Other Parts Discussed in Thread: DAC53701 , DAC53002 Hello,
Please can you share Gain Drift & Zero-Code Error Drift for DAC53202.
Also, please confirm what is the max output load driving capability of DAC53202.
Part Number: DAC53202 Other Parts Discussed in Thread: LM3243
Hello,
I'm currently using a DAC53202 and controlling it with SPI.
I want to control Buck's output voltage slew rate by connecting the output of DAC53202's OUT1 to LM3243's VCON.
I…
Part Number: DAC53202 Hi,
I‘am using DAC53202,the output current and voltage of the DAC can be correctly changed by configuring the DAC-X-DATA, but when trying to read back any register, the SDO pin is always at the IO level.
The clock cycle of the…
Part Number: DAC53202 Other Parts Discussed in Thread: DAC63204EVM , INA228 , SYSCONFIG
I'm trying to bringup DAC53202 with nRF52840 any reference for that...!
Part Number: DAC53202 Im attempting to ensure that I can successfully change the output voltage. My procedure is below:
Set the common config to 0x800
Set dac0 and dac1 cmp config value (identically set to 0x8000)
Set the dac output values
…
Part Number: DAC53202 For a DC/DC circuit that outputs negative voltage, is it feasible to adjust the negative rail by changing the magnitude of the current from the source current of the DAC and passing it through the resistor between FB and VOUT, and…