Part Number: DAC53204 Hello,
1) MCU IO is 3.3V, but DAC Vout is 0~5V. So the SPI pull up is connected to 3.3V, and VDD is connected to 5V, is it ok?
2) To protect Vout if short to 16V or GND, added 1k resistor as below, any concern?
3) If you use…
Part Number: DAC53204 Other Parts Discussed in Thread: INA181 Hello,
Use DAC53204 as Voltage output mode to generate E load design concept.
And use below INA181 for feedback, please confirm if there is any issue for it as it has gain =20.
The purpose…
Part Number: DAC53204 Other Parts Discussed in Thread: DAC63204 Tool/software: Hi,
I'm using this DAC53204(Current output mode) in our design.
1.If I need to margin the voltage with +/-10%, How the manual calculation will be?'
2.If I set DAC code…
Part Number: DAC53204 Tool/software: Hello,
I would like to use below concept to realise eload application from 0~2A.
1) in datasheet, there is CL max 200pF. Does it means external MOSFET gate input capacitance should be small than it?
If yes, please…
Part Number: DAC53204 Due to a certain reason, I am unable to generate a sawtooth wave at a frequency of 25 kHz (for PWM signal using feedback) I would appreciate assistance in achieving the desired configuration to reach this frequency
Ariel
Part Number: DAC53204 Hello,
I work with the DAC53204 for voltage margining and scaling. I designed the circuit according to the VOUT MODE with External Ref and relied on your application note on the subject.
Every few cycles of writing word-to-data_out…
Part Number: DAC53204-Q1 Other Parts Discussed in Thread: DAC53204 Tool/software: Hi team,
My customer wants a sine wave generator and they need 20 channel sine wave with 12V RMS and 10mA output current capacity.
They also need to control the frequency…