Part Number: DAC53204 Other Parts Discussed in Thread: DAC63204 Tool/software: Hi,
I'm using this DAC53204(Current output mode) in our design.
1.If I need to margin the voltage with +/-10%, How the manual calculation will be?'
2.If I set DAC code…
Part Number: DAC53204 Tool/software: Hello,
I would like to use below concept to realise eload application from 0~2A.
1) in datasheet, there is CL max 200pF. Does it means external MOSFET gate input capacitance should be small than it?
If yes, please…
Part Number: DAC53204 Due to a certain reason, I am unable to generate a sawtooth wave at a frequency of 25 kHz (for PWM signal using feedback) I would appreciate assistance in achieving the desired configuration to reach this frequency
Ariel
Part Number: DAC53204-Q1 Other Parts Discussed in Thread: DAC53204 Tool/software: Hi team,
My customer wants a sine wave generator and they need 20 channel sine wave with 12V RMS and 10mA output current capacity.
They also need to control the frequency…
Part Number: DAC53204 Hello,
I work with the DAC53204 for voltage margining and scaling. I designed the circuit according to the VOUT MODE with External Ref and relied on your application note on the subject.
Every few cycles of writing word-to-data_out…
Part Number: DAC53204 Tool/software: Hello,
I am trying to get proper communication with my DAC53204 device and believe I am sending the proper commands in order to enter 4-Wire SPI mode. The issue is that I am never seeing a Write Command echo on my…
Part Number: DAC53204 Tool/software: Hi,
I am using the echo (readback ?) mode of the DAC53204, but in the echo frame it is like if the first bit (MSB) was set to 1 altough sent 0 (write command).
Here, I send write on 0x26 and it echoes 0xA6 which…
Part Number: DAC53204 Tool/software: Hi,
I am getting the DAC53204 to work, and I am questionning the sense of the phrase "The SPI clock speed in readback mode is slower than that in write mode.", which is repeated several times in the DS.
For me…