Part Number: DAC53204-Q1 Other Parts Discussed in Thread: DAC53204 , DAC539G2-Q1 , , DAC53701-Q1
Hi team,
My customer requires 2ch PWM signal for LED indicator. DAC53204 should be a candidate for such application. Can DAC53204 be used for such application…
Part Number: DAC53204 Hi,
The datasheet for the DAC53204YBHR shows 12b codes for the sinewave generation function (page 42). Is there an equivalent for the 10b variant of this DAC family?
Thanks!
Part Number: DAC53204 Hi Team,
We would like to ask your help regarding our customer's inquiry below.
I used the 10bits DAC53204 on my board. Looked into the datasheet, still need help on the following:
I tried to write a look up table into the…
Part Number: DAC53204 Other Parts Discussed in Thread: DAC63204 Hello,
Regarding SPI Programming mode at 7.5.1
The slot for the register address is 7 bit long but register address is 8 bit long, example (table 7-21):
Do we need to chump the…
Part Number: DAC53204
Hi,
My board has two DACs with the SPI connected in a daisy chain. We are unable to program the 2nd DAC in the chain. There are 3 relevant pieces of information:
a) The DACs power up in 3-wire SPI mode (i.e daisy chain is…
Part Number: DAC53204 Hi
Is there any protection/limitation If voltage is applied through a 20K pull-up resistor to GPIO pin when the DAC53204VDD is 0?
Same regarding the I2C, what if the I2C pull up is connected to a different voltage that is not…
Part Number: DAC53204W Other Parts Discussed in Thread: DAC53204 Tool/software: Target application: to achieve PWM current source, 5mA/0.5ms, 20mA/0.5ms, 1KHz PWM.
schematic: VDD=3.3V, MOSFET gsth = 0.9V, Rset = 51ohm, use internal reference.
software…
Part Number: LM10011 Other Parts Discussed in Thread: DAC63204 , DAC53204 Tool/software: Hi team,
do we have newer device for LM10011? detail question as below:
Question ①: Is there any new solution for Vout voltage regulation? Question ②: Is there…
Part Number: DAC7311 Other Parts Discussed in Thread: DAC53204 Tool/software: We would like to use a DAC for scaling the voltage of a SMPS via current-injection into the feedback pin, however in our application the SMPS output may be externally powered…